![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.01
|
Data Fields | |
| unsigned int | bonding:2 |
| Bonding flags. More... | |
| unsigned int | ct2:1 |
| h7 Link Key conversion support (not used in LE) More... | |
| unsigned int | kp:1 |
| LE SC Keypress Notifications. More... | |
| unsigned int | mitm:1 |
| Man-In-The-Middle (MITM) More... | |
| unsigned int | reserved:2 |
| Reserved - don't use. More... | |
| unsigned int | sc:1 |
| LE Secure Connections (SC) More... | |
Pairing Request & Response - authReq field
| unsigned int bonding |
Bonding flags.
| unsigned int ct2 |
h7 Link Key conversion support (not used in LE)
| unsigned int kp |
LE SC Keypress Notifications.
| unsigned int mitm |
Man-In-The-Middle (MITM)
| unsigned int reserved |
Reserved - don't use.
| unsigned int sc |
LE Secure Connections (SC)