![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.01
|
Prepare Write Request format. More...
Data Fields | |
| uint16 | handle |
| Handle of the attribute to be written (must be first field) More... | |
| uint16 | len |
| Length of value. More... | |
| uint16 | offset |
| Offset of the first octet to be written. More... | |
| uint8 * | pValue |
| Part of the value of the attribute to be written (0 to ATT_MTU_SIZE-5) - must be allocated. More... | |
Prepare Write Request format.
for method ATT_PREPARE_WRITE_REQ
| uint16 handle |
Handle of the attribute to be written (must be first field)
| uint16 len |
Length of value.
| uint16 offset |
Offset of the first octet to be written.
| uint8* pValue |
Part of the value of the attribute to be written (0 to ATT_MTU_SIZE-5) - must be allocated.