![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.01
|
Attribute Protocol PDU format. More...
Data Fields | |
| uint8 | cmd |
| Command Flag. More... | |
| uint16 | len |
| Length of Attribute Parameters. More... | |
| uint8 | method |
| Method. More... | |
| uint8 * | pParams |
| Attribute Parameters. More... | |
| uint8 | sig |
| Authentication Signature status (not included (0), valid (1), invalid (2)) More... | |
Attribute Protocol PDU format.
| uint8 cmd |
Command Flag.
| uint16 len |
Length of Attribute Parameters.
| uint8 method |
Method.
| uint8* pParams |
Attribute Parameters.
| uint8 sig |
Authentication Signature status (not included (0), valid (1), invalid (2))