![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.01
|
GATT Attribute format. More...
Data Fields | |
| uint16 | handle |
| Attribute handle - assigned internally by attribute server. More... | |
| uint8 | permissions |
| Attribute permissions. More... | |
| uint8 *const | pValue |
| gattAttrType_t | type |
| Attribute type (2 or 16 octet UUIDs) More... | |
GATT Attribute format.
| uint16 handle |
Attribute handle - assigned internally by attribute server.
| uint8 permissions |
Attribute permissions.
| uint8* const pValue |
Attribute value - encoding of the octet array is defined in the applicable profile. The maximum length of an attribute value shall be 512 octets.
| gattAttrType_t type |
Attribute type (2 or 16 octet UUIDs)