TI BLE5-Stack API Documentation  9.14.01
Data Fields
CS_setProcedureParamsCmdParams_t Struct Reference

Data Fields

csACI_e aci
 Antenna Configuration Index csACI_e. More...
 
uint8_t configID
 Configuration ID. More...
 
uint16_t connHandle
 Connection handle. More...
 
uint8_t enable
 Is procedure enabled CS_Enable. More...
 
uint16_t maxProcedureCount
 Maximum number of CS procedures to be scheduled (0 - indefinite) More...
 
uint16_t maxProcedureDur
 Maximum procedure duration in 0.625 milliseconds. More...
 
uint16_t maxProcedureInterval
 Maximum number of connection events between consecutive CS procedures. More...
 
uint32_t maxSubEventLen
 Maximum SubEvent length in microseconds, range 1250us to 4s. More...
 
uint16_t minProcedureInterval
 Minimum number of connection events between consecutive CS procedures. More...
 
uint32_t minSubEventLen
 Minimum SubEvent length in microseconds, range 1250us to 4s. More...
 
uint8_t phy
 PHY CS_Phy_Supported. More...
 
uint8_t preferredPeerAntenna
 Preferred peer antenna. More...
 
uint8_t snrCtrlI
 SNR Control Initiator. More...
 
uint8_t snrCtrlR
 SNR Control Reflector. More...
 
uint8_t txPwrDelta
 Tx Power Delta, in signed dB. More...
 

Field Documentation

§ aci

csACI_e aci

Antenna Configuration Index csACI_e.

§ configID

uint8_t configID

Configuration ID.

§ connHandle

uint16_t connHandle

Connection handle.

§ enable

uint8_t enable

Is procedure enabled CS_Enable.

§ maxProcedureCount

uint16_t maxProcedureCount

Maximum number of CS procedures to be scheduled (0 - indefinite)

§ maxProcedureDur

uint16_t maxProcedureDur

Maximum procedure duration in 0.625 milliseconds.

§ maxProcedureInterval

uint16_t maxProcedureInterval

Maximum number of connection events between consecutive CS procedures.

§ maxSubEventLen

uint32_t maxSubEventLen

Maximum SubEvent length in microseconds, range 1250us to 4s.

§ minProcedureInterval

uint16_t minProcedureInterval

Minimum number of connection events between consecutive CS procedures.

§ minSubEventLen

uint32_t minSubEventLen

Minimum SubEvent length in microseconds, range 1250us to 4s.

§ phy

uint8_t phy

PHY CS_Phy_Supported.

§ preferredPeerAntenna

uint8_t preferredPeerAntenna

Preferred peer antenna.

§ snrCtrlI

uint8_t snrCtrlI

SNR Control Initiator.

§ snrCtrlR

uint8_t snrCtrlR

SNR Control Reflector.

§ txPwrDelta

uint8_t txPwrDelta

Tx Power Delta, in signed dB.


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale