TI BLE5-Stack API Documentation  9.14.01
Data Fields
CS_readRemoteCapabEvt_t Struct Reference

Data Fields

uint8_t chSel3c
 channel selection 3c support More...
 
uint16_t connHandle
 connection handle More...
 
uint8_t csBasedRanging
 CS based ranging. More...
 
csEventOpcodes_e csEvtOpcode
 CS Event Code csEventOpcodes_e. More...
 
uint8_t csStatus
 Event status. More...
 
uint8_t maxAntPath
 max number of antenna paths that are supported More...
 
uint16_t maxProcedures
 Max num of CS procedures supported. More...
 
uint16_t nadmRandomSeq
 NADM Random Sequence Capability. More...
 
uint16_t nadmSounding
 NADM Sounding Capability. More...
 
uint8_t noFAE
 No FAE. More...
 
uint8_t numAntennas
 the number of antenna elements that are available for CS tone exchanges More...
 
uint8_t numConfig
 Number of CS configurations supported per conn. More...
 
uint8_t optionalCsSyncPhy
 supported CS sync PHYs, bit mapped field More...
 
uint8_t optionalModes
 indicates which of the optional CS modes are supported More...
 
uint8_t role
 initiator or reflector CS_Role More...
 
uint8_t rttAAOnlyN
 Number of CS steps of single packet exchanges needed. More...
 
uint8_t rttCap
 indicate which of the time-of-flight accuracy requirements are met More...
 
uint8_t rttRandomPayloadN
 Num of CS steps of single packet exchange needed. More...
 
uint8_t rttSoundingN
 Number of CS steps of single packet exchanges needed. More...
 
uint8_t snrTxCap
 Spec defines an additional byte for RFU. More...
 
uint16_t tFcsCap
 tFCS Capability More...
 
uint16_t tIp1Cap
 tIP1 Capability More...
 
uint16_t tIp2Cap
 tTP2 Capability More...
 
uint16_t tPmCsap
 tPM Capability More...
 
uint8_t tSwCap
 Antenna switch time capability. More...
 

Field Documentation

§ chSel3c

uint8_t chSel3c

channel selection 3c support

§ connHandle

uint16_t connHandle

connection handle

§ csBasedRanging

uint8_t csBasedRanging

CS based ranging.

§ csEvtOpcode

csEventOpcodes_e csEvtOpcode

CS Event Code csEventOpcodes_e.

§ csStatus

uint8_t csStatus

Event status.

§ maxAntPath

uint8_t maxAntPath

max number of antenna paths that are supported

§ maxProcedures

uint16_t maxProcedures

Max num of CS procedures supported.

§ nadmRandomSeq

uint16_t nadmRandomSeq

NADM Random Sequence Capability.

§ nadmSounding

uint16_t nadmSounding

NADM Sounding Capability.

§ noFAE

uint8_t noFAE

No FAE.

§ numAntennas

uint8_t numAntennas

the number of antenna elements that are available for CS tone exchanges

§ numConfig

uint8_t numConfig

Number of CS configurations supported per conn.

§ optionalCsSyncPhy

uint8_t optionalCsSyncPhy

supported CS sync PHYs, bit mapped field

§ optionalModes

uint8_t optionalModes

indicates which of the optional CS modes are supported

§ role

uint8_t role

initiator or reflector CS_Role

§ rttAAOnlyN

uint8_t rttAAOnlyN

Number of CS steps of single packet exchanges needed.

§ rttCap

uint8_t rttCap

indicate which of the time-of-flight accuracy requirements are met

§ rttRandomPayloadN

uint8_t rttRandomPayloadN

Num of CS steps of single packet exchange needed.

§ rttSoundingN

uint8_t rttSoundingN

Number of CS steps of single packet exchanges needed.

§ snrTxCap

uint8_t snrTxCap

Spec defines an additional byte for RFU.

§ tFcsCap

uint16_t tFcsCap

tFCS Capability

§ tIp1Cap

uint16_t tIp1Cap

tIP1 Capability

§ tIp2Cap

uint16_t tIp2Cap

tTP2 Capability

§ tPmCsap

uint16_t tPmCsap

tPM Capability

§ tSwCap

uint8_t tSwCap

Antenna switch time capability.


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale