TI BLE5-Stack API Documentation  9.14.01
Data Fields
CS_procEnableCompleteEvt_t Struct Reference

Data Fields

csACI_e ACI
 Antenna Config Index csACI_e. More...
 
uint8_t configId
 configuration ID More...
 
uint16_t connHandle
 connection handle More...
 
csEventOpcodes_e csEvtOpcode
 CS Event Code. More...
 
uint8_t csStatus
 Event status. More...
 
uint8_t enable
 enable/disable CS_Enable More...
 
uint16_t eventInterval
 event interval in units of connection interval More...
 
uint16_t procedureCount
 procedure count More...
 
uint16_t procedureInterval
 procedure interval More...
 
int8_t selectedTxPower
 Transmit power level used for CS procedure. Units: dBm. More...
 
uint16_t subEventInterval
 sub-event interval in units of 625 us More...
 
uint32_t subEventLen
 sub-event length in microseconds, range 1250us to 4s More...
 
uint8_t subEventsPerEvent
 number of CS SubEvents in a CS Event More...
 

Field Documentation

§ ACI

csACI_e ACI

Antenna Config Index csACI_e.

§ configId

uint8_t configId

configuration ID

§ connHandle

uint16_t connHandle

connection handle

§ csEvtOpcode

csEventOpcodes_e csEvtOpcode

CS Event Code.

§ csStatus

uint8_t csStatus

Event status.

§ enable

uint8_t enable

enable/disable CS_Enable

§ eventInterval

uint16_t eventInterval

event interval in units of connection interval

§ procedureCount

uint16_t procedureCount

procedure count

§ procedureInterval

uint16_t procedureInterval

procedure interval

§ selectedTxPower

int8_t selectedTxPower

Transmit power level used for CS procedure. Units: dBm.

§ subEventInterval

uint16_t subEventInterval

sub-event interval in units of 625 us

§ subEventLen

uint32_t subEventLen

sub-event length in microseconds, range 1250us to 4s

§ subEventsPerEvent

uint8_t subEventsPerEvent

number of CS SubEvents in a CS Event


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale