TI BLE5-Stack API Documentation  9.14.01
Data Fields
CS_configCompleteEvt_t Struct Reference

Data Fields

uint8_t ch3CJump
 one of the valid CSChannelJump values More...
 
uint8_t ch3cShape
 selected shape to be rendered More...
 
csChm_t channelMap
 channel map csChm_t More...
 
uint8_t chMRepetition
 number of times the ChM field will be cycled through More...
 
uint8_t chSel
 channel selection algorithm to be used CS_Chan_Sel_Alg More...
 
uint8_t configId
 CS configuration ID. More...
 
uint16_t connHandle
 connection handle More...
 
csEventOpcodes_e csEvtOpcode
 CS Event Code. More...
 
uint8_t csStatus
 Event status. More...
 
uint8_t csSyncPhy
 transmit and receive PHY to be used CS_Sync_Phy_Supported More...
 
uint8_t mainMode
 which CS modes are to be used CS_Mode More...
 
uint8_t mainModeMaxSteps
 a Sub_Mode step is executed More...
 
uint8_t mainModeMinSteps
 range of Main_Mode steps to be executed before More...
 
uint8_t mainModeRepetition
 num of main mode steps from the last CS subevent to be repeated More...
 
uint8_t modeZeroSteps
 number of mode 0 steps to be included at the beginning of each CS Subevent More...
 
uint8_t rfu0
 reserved for future use More...
 
uint8_t rfu1
 reserved for future use More...
 
uint8_t role
 initiator or reflector CS_Role More...
 
uint8_t rttType
 which RTT variant is to be used CS_RTT_Type More...
 
uint8_t state
 0b00 disabled, 0b01 enabled More...
 
uint8_t subMode
 which CS modes are to be used CS_Mode More...
 
uint8_t tFCs
 Index used for frequency changes. More...
 
uint8_t tIP1
 Index of the period used between RTT packets. More...
 
uint8_t tIP2
 Index of the interlude period used between CS tones. More...
 
uint8_t tPM
 Index for the measurement period of CS tones. More...
 

Field Documentation

§ ch3CJump

uint8_t ch3CJump

one of the valid CSChannelJump values

§ ch3cShape

uint8_t ch3cShape

selected shape to be rendered

§ channelMap

csChm_t channelMap

channel map csChm_t

§ chMRepetition

uint8_t chMRepetition

number of times the ChM field will be cycled through

§ chSel

uint8_t chSel

channel selection algorithm to be used CS_Chan_Sel_Alg

§ configId

uint8_t configId

CS configuration ID.

§ connHandle

uint16_t connHandle

connection handle

§ csEvtOpcode

csEventOpcodes_e csEvtOpcode

CS Event Code.

§ csStatus

uint8_t csStatus

Event status.

§ csSyncPhy

uint8_t csSyncPhy

transmit and receive PHY to be used CS_Sync_Phy_Supported

§ mainMode

uint8_t mainMode

which CS modes are to be used CS_Mode

§ mainModeMaxSteps

uint8_t mainModeMaxSteps

a Sub_Mode step is executed

§ mainModeMinSteps

uint8_t mainModeMinSteps

range of Main_Mode steps to be executed before

§ mainModeRepetition

uint8_t mainModeRepetition

num of main mode steps from the last CS subevent to be repeated

§ modeZeroSteps

uint8_t modeZeroSteps

number of mode 0 steps to be included at the beginning of each CS Subevent

§ rfu0

uint8_t rfu0

reserved for future use

§ rfu1

uint8_t rfu1

reserved for future use

§ role

uint8_t role

initiator or reflector CS_Role

§ rttType

uint8_t rttType

which RTT variant is to be used CS_RTT_Type

§ state

uint8_t state

0b00 disabled, 0b01 enabled

§ subMode

uint8_t subMode

which CS modes are to be used CS_Mode

§ tFCs

uint8_t tFCs

Index used for frequency changes.

§ tIP1

uint8_t tIP1

Index of the period used between RTT packets.

§ tIP2

uint8_t tIP2

Index of the interlude period used between CS tones.

§ tPM

uint8_t tPM

Index for the measurement period of CS tones.


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale