![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.01
|
BLEAppUtil General Params Structure. More...
Data Fields | |
| GAP_Addr_Modes_t | addressMode |
| uint16_t | appearanceAtt |
| Appearance attribute. More... | |
| uint8_t * | deviceNameAtt |
| Device name attribute. More... | |
| uint8_t * | pDeviceRandomAddress |
| gapPeriConnectParams_t | periConnParamsAtt |
| Peripheral Preferred Connection Parameters. More... | |
| BLEAppUtil_Profile_Roles_e | profileRole |
| Profile role. roles are defined at BLEAppUtil_Profile_Roles_e. More... | |
| int | taskPriority |
| Task priority. More... | |
| size_t | taskStackSize |
| Task stack size. More... | |
BLEAppUtil General Params Structure.
Should be created by the application and passed to BLEAppUtil_init.
| GAP_Addr_Modes_t addressMode |
Own address mode. If always using Resolvable Private Address, set this to either ADDRMODE_RP_WITH_PUBLIC_ID or ADDRMODE_RP_WITH_RANDOM_ID. If always using Identity Address, set this to either ADDRMODE_PUBLIC or ADDRMODE_RANDOM.
| uint16_t appearanceAtt |
Appearance attribute.
| uint8_t* deviceNameAtt |
Device name attribute.
| uint8_t* pDeviceRandomAddress |
Pointer to 6-byte Random Static Address of this device that will be copied to the stack. Valid only if addrMode is ADDRMODE_RANDOM or ADDRMODE_RP_WITH_RANDOM_ID and can not be NULL in these cases. Ignored for other address types.
| gapPeriConnectParams_t periConnParamsAtt |
Peripheral Preferred Connection Parameters.
| BLEAppUtil_Profile_Roles_e profileRole |
Profile role. roles are defined at BLEAppUtil_Profile_Roles_e.
| int taskPriority |
Task priority.
| size_t taskStackSize |
Task stack size.