![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.01
|
Macros | |
| #define | GAP_ADV_REMOVE_SET_EVENT 0x13 |
| Sent when an advertising set needs to be removed. This is an internal event. More... | |
| #define | GAP_ADV_SET_PERIODIC_ADV_DATA_EVENT 0x1A |
| Set periodic advertising data command complete event. More... | |
| #define | GAP_ADV_SET_PERIODIC_ADV_ENABLE_EVENT 0x1B |
| Set periodic advertising enable command complete event. More... | |
| #define | GAP_ADV_SET_PERIODIC_ADV_PARAMS_EVENT 0x19 |
| Set periodic advertising parameters command complete event. More... | |
| #define | GAP_AUTHENTICATION_COMPLETE_EVENT 0x0A |
| #define | GAP_AUTHENTICATION_FAILURE_EVT 0x10 |
| #define | GAP_BOND_COMPLETE_EVENT 0x0E |
| #define | GAP_BOND_LOST_EVENT 0x17 |
| #define | GAP_CONNECTING_CANCELLED_EVENT 0x15 |
| #define | GAP_DEVICE_INIT_DONE_EVENT 0x00 |
| #define | GAP_LINK_ESTABLISHED_EVENT 0x05 |
| #define | GAP_LINK_PARAM_UPDATE_EVENT 0x07 |
| #define | GAP_LINK_PARAM_UPDATE_REJECT_EVENT 0x18 |
| #define | GAP_LINK_TERMINATED_EVENT 0x06 |
| #define | GAP_PAIRING_REQ_EVENT 0x0F |
| #define | GAP_PASSKEY_NEEDED_EVENT 0x0B |
| #define | GAP_PERIPHERAL_REQUESTED_SECURITY_EVENT 0x0C |
| #define | GAP_SCAN_ADD_DEVICE_ADV_LIST_EVENT 0x20 |
| Add device to period advertisers list command complete event. More... | |
| #define | GAP_SCAN_CLEAR_ADV_LIST_EVENT 0x23 |
| Clear period advertisers list command complete event. More... | |
| #define | GAP_SCAN_CREATE_SYNC_EVENT 0x1C |
| #define | GAP_SCAN_PERIODIC_ADV_REPORT_EVENT 0x26 |
| #define | GAP_SCAN_PERIODIC_ADV_SYNC_EST_EVENT 0x24 |
| #define | GAP_SCAN_PERIODIC_ADV_SYNC_LOST_EVENT 0x25 |
| #define | GAP_SCAN_PERIODIC_RECEIVE_EVENT 0x1F |
| Periodic advertising receive enable command complete event. More... | |
| #define | GAP_SCAN_READ_ADV_LIST_SIZE_EVENT 0x22 |
| Read period advertisers list size command complete event. More... | |
| #define | GAP_SCAN_REMOVE_DEVICE_ADV_LIST_EVENT 0x21 |
| Remove device from period advertisers list create sync command complete event. More... | |
| #define | GAP_SCAN_SESSION_END_EVENT 0x12 |
| Sent when an advertising report session ends. This is an internal event. More... | |
| #define | GAP_SCAN_SYNC_CANCEL_EVENT 0x1D |
| Periodic advertising create sync command complete event. More... | |
| #define | GAP_SCAN_TERMINATE_SYNC_EVENT 0x1E |
| Periodic advertising terminate sync command complete event. More... | |
| #define | GAP_SIGNATURE_UPDATED_EVENT 0x09 |
| #define | GAP_UPDATE_LINK_PARAM_REQ_EVENT 0x11 |
These events are received as GAP_MSG_EVENT
| #define GAP_ADV_REMOVE_SET_EVENT 0x13 |
Sent when an advertising set needs to be removed. This is an internal event.
| #define GAP_ADV_SET_PERIODIC_ADV_DATA_EVENT 0x1A |
Set periodic advertising data command complete event.
| #define GAP_ADV_SET_PERIODIC_ADV_ENABLE_EVENT 0x1B |
Set periodic advertising enable command complete event.
| #define GAP_ADV_SET_PERIODIC_ADV_PARAMS_EVENT 0x19 |
Set periodic advertising parameters command complete event.
Periodic Advertising Advertiser command complete events.
| #define GAP_AUTHENTICATION_COMPLETE_EVENT 0x0A |
Sent when the pairing process is complete as gapAuthCompleteEvent_t.
This event will be consumed by the gapbondmgr if it is present
| #define GAP_AUTHENTICATION_FAILURE_EVT 0x10 |
Sent when pairing fails due a connection termination before the process completed. This event does not have any payload.
This event will be consumed by the gapbondmgr if it is present.
| #define GAP_BOND_COMPLETE_EVENT 0x0E |
Sent when the bonding process is complete as gapBondCompleteEvent_t.
This event will be consumed by the gapbondmgr if it is present
| #define GAP_BOND_LOST_EVENT 0x17 |
Sent as gapBondLostEvent_t when bond has been removed on peer
| #define GAP_CONNECTING_CANCELLED_EVENT 0x15 |
Sent as gapConnCancelledEvent_t when an a connecting attempt is canceled
| #define GAP_DEVICE_INIT_DONE_EVENT 0x00 |
Sent after a call to GAP_DeviceInit when the Device Initialization is complete as gapDeviceInitDoneEvent_t.
| #define GAP_LINK_ESTABLISHED_EVENT 0x05 |
Sent after a link has been established as gapEstLinkReqEvent_t.
| #define GAP_LINK_PARAM_UPDATE_EVENT 0x07 |
Sent after the completion of a parameter update gapLinkUpdateEvent_t.
This same event is received for both the LL and L2CAP procedures.
| #define GAP_LINK_PARAM_UPDATE_REJECT_EVENT 0x18 |
Sent after a recieved Connection Parameter Update Request was rejected by this device.
| #define GAP_LINK_TERMINATED_EVENT 0x06 |
Sent when a connection was terminated as gapTerminateLinkEvent_t.
| #define GAP_PAIRING_REQ_EVENT 0x0F |
Sent when an unexpected Pairing Request is received as gapPairingReqEvent_t.
This event will be consumed by the gapbondmgr if it is present
| #define GAP_PASSKEY_NEEDED_EVENT 0x0B |
Sent when a passkey is needed during pairing as gapPasskeyNeededEvent_t.
This event will be consumed by the gapbondmgr if it is present
| #define GAP_PERIPHERAL_REQUESTED_SECURITY_EVENT 0x0C |
Sent when a Peripheral Security Request is received as gapPeripheralSecurityReqEvent_t.
This event will be consumed by the gapbondmgr if it is present
| #define GAP_SCAN_ADD_DEVICE_ADV_LIST_EVENT 0x20 |
Add device to period advertisers list command complete event.
| #define GAP_SCAN_CLEAR_ADV_LIST_EVENT 0x23 |
Clear period advertisers list command complete event.
| #define GAP_SCAN_CREATE_SYNC_EVENT 0x1C |
Periodic Advertising Scanner command status event.
| #define GAP_SCAN_PERIODIC_ADV_REPORT_EVENT 0x26 |
Periodic Advertising Scanner report event.
| #define GAP_SCAN_PERIODIC_ADV_SYNC_EST_EVENT 0x24 |
Periodic Advertising Scanner establish event.
| #define GAP_SCAN_PERIODIC_ADV_SYNC_LOST_EVENT 0x25 |
Periodic Advertising Scanner sync lost event.
| #define GAP_SCAN_PERIODIC_RECEIVE_EVENT 0x1F |
Periodic advertising receive enable command complete event.
| #define GAP_SCAN_READ_ADV_LIST_SIZE_EVENT 0x22 |
Read period advertisers list size command complete event.
| #define GAP_SCAN_REMOVE_DEVICE_ADV_LIST_EVENT 0x21 |
Remove device from period advertisers list create sync command complete event.
| #define GAP_SCAN_SESSION_END_EVENT 0x12 |
Sent when an advertising report session ends. This is an internal event.
| #define GAP_SCAN_SYNC_CANCEL_EVENT 0x1D |
Periodic advertising create sync command complete event.
Periodic Advertising Scanner command complete events.
| #define GAP_SCAN_TERMINATE_SYNC_EVENT 0x1E |
Periodic advertising terminate sync command complete event.
| #define GAP_SIGNATURE_UPDATED_EVENT 0x09 |
Sent when the peer device's signature counter is updated as gapSignUpdateEvent_t.
This event will be consumed by the gapbondmgr if it is present
| #define GAP_UPDATE_LINK_PARAM_REQ_EVENT 0x11 |
Sent when a parameter update request is received. This event is only received when GAP_PARAM_LINK_UPDATE_DECISION is set to GAP_UPDATE_REQ_PASS_TO_APP. This event is sent as gapUpdateLinkParamReqEvent_t.