Changelog

Table of Contents

 

New Features

BLE Stack

ID Summary
BLE_LOKI-3836 Add Connection Parameter Update Event Handler to Car Node Example
BLE_LOKI-3819 Reduce the Number of Steps within TX Double Buffer for Channel Sounding
BLE_LOKI-3801 Add Connection Parameter Update APIs
BLE_LOKI-3798 Implement RAS/RAP Real Time Client
BLE_LOKI-3786 Add Support for L2CAP Send SDU Flow Control with Channel Sounding
BLE_LOKI-3754 Support Central Mode on Key Node Example
BLE_LOKI-3629 Support Initializing of Multiple Generated Advertising Sets in SysConfig

TI Proprietary RF

ID Summary
None None

TI Zigbee

ID Summary
None None
ID Summary
SCCM-592 CC27XX HSM BareMetal module shall support Asymmetric Asset operations
SCCM-591 CC27XX HSM BareMetal Module shall support one key blob element

Core SDK

ID Summary
LPRFXXWARE-1072 Add UART2 LIN HAL-support

Radio Control Library (RCL)

ID Summary
RCL-1257 BLE CS: Improve Tx tone quality for multiple antenna configuration

 

Fixed Issues

BLE Stack

ID Summary
BLE_LOKI-3849 Reject Connection Parameter Update Request from Peer during CS Procedure
BLE_LOKI-3840 Scanner cannot Find Device that Distributes IRK with Static Random Address after Bonding and Reset
BLE_LOKI-3837 Fix Synchronization - Procedure Counter not Incremented when Reject Packet Sent/Received
BLE_LOKI-3820 Adjust Peripheral startTime in Case we Miss the Peer on the CS Instant
BLE_LOKI-3808 Repeated calls to CS_GetRole floods the BLE Stack message queue
BLE_LOKI-3807 Scheduling Stops when Device Disconnects During Channel Sounding
BLE_LOKI-3800 Channel Sounding may Lose Synchronization of Procedure Counter when Multiple Tasks are Active
BLE_LOKI-3795 BLE Stack Might Hang when Adv/Scan Executes Before the CS Procedure
BLE_LOKI-3794 Channel Sounding CS_SUBEVENT may Report Incorrect Connection Handle
BLE_LOKI-3793 BLE Stack Scheduler Time Comparison Causes Channel Sounding to Crash
BLE_LOKI-3790 Large CS_OFFSET Value Causes Reflector to Miss the Start Procedure
BLE_LOKI-3789 Bluetooth Health Thermometer Profile uses Incorrect Data Format
BLE_LOKI-3788 No GAP_EVT_SCAN_ENABLED Events when only Selected Observer Role in SysCfg

TI Proprietary RF

ID Summary
None None

TI Zigbee

ID Summary
TI_ZIGBEE-260 Hardcoded 50ms delay between fragmented packets
ID Summary
SCCM-621 Extra trailer length of 0x630 getting introduced

Core SDK

ID Summary
TIDRIVERS-7596 APULPF3_dataMemTransfer fails when source and destination is in APU memory

Radio Control Library (RCL)

ID Summary
None None

 

Known Issues

BLE Stack

ID Summary
BLE_LOKI-3872 Distance not Reported for One or More Keys During Multiple Connections
BLE_LOKI-3869 Looping Through CM Start and CM Stop Causes Channel Sounding Failure
BLE_LOKI-3828 CS Procedure may be Aborted if Received Data Length/Time Exceeds CS_OFFSET
BLE_LOKI-3724 IAR Compiler Error when Compiling Basic_persistent on CC2340 Devices
BLE_LOKI-3676 Channel Sounding Timeout Distance Events for Mode 3 with 2x2 Antennas
BLE_LOKI-3536 If parameter update or channel map update w/ CSA#1 is from the past - Connection Monitor will terminate
BLE_LOKI-3535 Connection Monitor Cannot properly track connection on Coded PHY
BLE_LOKI-3473 IAR Compiled Car Node and Key Node Executing Channel Sounding in Loops Causes GAP Link Termination
BLE_LOKI-3429 No Distance is Received after 160 to 255 CS Procedures using RAS over Indications
BLE_LOKI-3389 CS procedure must be complete before starting the next one
BLE_LOKI-3236 Calling HCI_ResetCmd Causes Program to Crash
BLE_LOKI-3208 BLE Agent GUI not able to calculate time offset correctly when running connection handover demo which causes frequent unsuccessful handover sessions
BLE_LOKI-3177 [SWAT] Observer failed to receive GAP_EVT_SCAN_DISABLED event
BLE_LOKI-3097 After changing PHY both devices continue to send Power Reporting events
BLE_LOKI-2978 Connnection Handover AuthenticationComplete Event Received after Handover When Candidate Configured To Initiate Pairing Request
BLE_LOKI-2842 CC23XX and CC27XX family of devices rounds down Tx power values that are not in the power table
BLE_LOKI-2650 CC2745R10Q1 Central Role Fails to Switch Connection PHY to Coded While Holding 16 Connections
BLE_LOKI-2648 Connection may be unstable with Coded PHY when Access Address has high cross-correlation with the preamble
BLE_LOKI-2373 CC2340R5 MAX periodic adv list size is hard coded and can't be configure by SysConfig
BLE_LOKI-2358 CC2340R5 Basic MR printed peripheral initial RPA after bond and pair, instead of its Public Address
BLE_LOKI-2108 Specific smart phone doesn't find peer running extended ADV with secondary PHY of 1M
BLE_LOKI-1630 Extended Advertisement Reports Are Not Filtered When SCAN_PARAM_FLT_DUP is Enabled

TI Proprietary RF

ID Summary
None None

TI Zigbee

ID Summary
None None
ID Summary
None None

Core SDK

ID Summary
TIDRIVERS-7475 I2S driver should not be used simultaneously with CAN or APU driver
TIDRIVERS-7416 The Power driver does not handle SysTimer channel 5 for CC27XX
TIDRIVERS-7244 Changing the muxing on an IO can cause glitches under some conditions
TIDRIVERS-7234 FPU registers not saved/restored around standby for NoRTOS/CM33
TIDRIVERS-7016 AESCCM/AESGCM driver do not support segmented finalize with no input when using HSM engine for CC27XX devices
TIDRIVERS-6863 JSON library unstable for gcc 12.3
LPRFSEC-250 PSA EDDSA+AES CBC,CCM,GCM,CMAC,CTR lack concurrent operation support

Radio Control Library (RCL)

ID Summary
None None