CC23xx or CC27xx SDK 9.11 to CC23xx or CC27xx SDK 9.14¶
This section will describe how to port a project from CC23xx or CC27xx SDK 9.11 to a CC23xx or CC27xx SDK 9.14 project.
Note
Vulnerability reports and mitigations can be found on Report potential product security vulnerabilities.
Porting Bluetooth LE Projects¶
The recommended method for porting an existing project from CC23xx or CC27xx SDK 9.11
to CC23xx or CC27xx SDK 9.14 is to modify the project using only the Code Composer Studio interface.
The following steps will detail the changes needed when porting an out of the box
example from the SDK such as basic_ble:
Import the project into Code Composer Studio.
2. In order to modify the SDK version, corresponding SysConfig version, as well as the compiler version,
right-click on the imported project folder inside the Project Explorer and select Properties.
3. In General, select Compiler and choose the correct version. Refer to the Dependencies section
in the SDK release notes
![]()
Figure 243. Code Composer Studio - Change Compiler Version.¶
4. Go to Dependencies and double-click on SimpleLink Low Power F3 SDK and choose the correct version.
Then double-click on SysConfig and do the same. Refer to the Dependencies Section in the SDK release notes
for the correct versions.
![]()
Figure 244. Code Composer Studio - Change SDK and SysConfig Version.¶
5. Add the necessary files to common->lib_opt folders. Right click on the lib_opt folder and select Add Files/Folders.
![]()
Figure 245. Code Composer Studio - Add Files to CCS Project.¶
6. Click the + button on the top right of the pop up screen. Next navigate to the lib_opt folder in the 9.14 SDK. Select the ellipses … button and navigate to the lib_opt folder in the 9.14 SDK.
![]()
Figure 246. Code Composer Studio - Select File Path Selection.¶
7. Navigate to COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR/source/ti/ble/stack_util/lib_opt/src and select all the files in the folder. These include ctrl_opt_dmm_dynamic_priority.c, ctrl_opt_dmm.c, ctrl_opt_ext_vendor_specific_cmd.c, ctrl_opt_past_receiver.c, ctrl_opt_past_sender.c, ctrl_opt_pawr_scan.c , and ctrl_opt_vendor_specific_cmd.c.
8. Follow steps 5-7 for the HealthToolKit->inc and HealthToolKit folders. Add files ble_sys_stat.h within the COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR/source/ti/ble/stack_util/health_toolkit folder, and ble_sys_stat.c within COM_TI_SIMPLELINK_LOWPOWER_F3_SDK_INSTALL_DIR/source/ti/ble/stack_util/health_toolkit/src folder.
9. The HSM firmware version has been updated from 3.0.0 to 3.1.1 for the CC23xx or CC27xx SDK 9.14 SDK release. Update the HSM firmware using Uniflash or Code Composer Studio.
If the newest SDK is not available, it will need to be actualized. To do this, go to File => Preferences
=> Code Composer Studio Settings, and select Products. Inside the Products tab, press the refresh
button, which should discover the latest version of the SDK that was installed.
A Few Noteworthy Changes from CC23xx or CC27xx SDK 9.11 to CC23xx or CC27xx SDK 9.14¶
You can follow the guide above without addressing these updates; they are listed for your information only. All fine grained details might not be mentioned.
- API Changes include:
- Connection Monitor Role:
Connection Monitor API CMS_GetConnDataSize(void) returns uint8_t instead of uint16_t.
Connection Monitor API CMS_GetConnData(uint16_t connHandle, uint8_t *pData) adds uint32_t accessAddr to the CMS_GetConnData structure.
adjustmentEvtTries and cmConnectionMaskRole_e connRole removed from cmStartMonitorParams_t structure.
cmDataSize within cmStartMonitorParams_t has been changed from uint32_t to uint8_t.
cmReportEvt_t now contains two packets, with either CM_PKT_STATUS_NOT_RECEIVED, CM_PKT_VALID_CENTRAL, CM_PKT_VALID_PERIPHERAL or CM_PKT_STATUS_UNDETERMINED status.
The size of Connection Monitor data is now 56 bytes.
- GapBondMgr:
- gapBondMgrReadBondRec has changed to GapBondMgr_readBondFromNv.
The function now takes four inputs instead of nine.
pSavedBondRec now contains all of the export bonding information.
See Extract Bonding Information for more details.
- Channel Sounding:
CS_writeRemoteFAETable(CS_writeRemoteFAETableParams_t *pParams) has changed to CS_writeCachedRemoteFAETable(CS_writeCachedRemoteFAETableParams_t *pParams) within cs.h.
ChannelSounding_writeRemoteFAETable(ChannelSounding_writeRemoteFAETableParams_t *pParams) has been changed to ChannelSounding_writeCachedRemoteFAETable(ChannelSounding_writeCachedRemoteFAETable *pParams) within app_cs.h and app_cs.c.
Function CS_WriteCachedRemoteSupportedCapabilities(CS_writeCachedRemoteSupportedCapabilitiesParams_t *pParams) has been added to cs.h.
Function ChannelSounding_writeCachedRemoteSupportedCapabilities (ChannelSounding_writeCachedRemoteSupportedCapabilitiesParams_t *pParams) has been added into app_cs.c.
Note
When porting to CC2744R7-Q1, the NVS region must be changed to reflect the flash size decrease from CC2745R10-Q1 to CC2744R7-Q1. If the NVS region is not altered, the application will enter the exception handler.
Please refer to the BLE5-Stack Release Notes for all the details.