API Documentation  9.14.01
Data Fields
PDMCC26XX_I2S_StreamNotification Struct Reference

A PDMCC26XX_I2S_StreamNotification data structure is used with PDMCC26XX_I2S_CallbackFxn(). Provides notification about available buffers and potential errors. More...

Data Fields

void * arg
 
PDMCC26XX_I2S_Status status
 

Detailed Description

A PDMCC26XX_I2S_StreamNotification data structure is used with PDMCC26XX_I2S_CallbackFxn(). Provides notification about available buffers and potential errors.

Field Documentation

§ arg

void* PDMCC26XX_I2S_StreamNotification::arg

Argument to be passed to the callback function

§ status

PDMCC26XX_I2S_Status PDMCC26XX_I2S_StreamNotification::status

Status code set by PDMCC26XX_I2S driver


The documentation for this struct was generated from the following file: