TI OAD API Documentation  9.14.01
File List
Here is a list of all documented files with brief descriptions:
 crypto.hPlatform Security Architecture cryptography module
 ext_flash_layout.hContains common structures and defines related to external flash layout as it for the OAD usecase
 flash_interface.hAn interface that abstracts flash operations for OAD this allows on-chip and off-chip OAD to use the same flash APIs
 HSMBareMetal.hInterface to The HSM IP in a BareMetal-based implementation
 oad_image_header.hStructure definition for image header and segments, these are prepended to the over the air images