TI BLE5-Stack API Documentation  9.14.01
Data Fields
l2capPacket_t Struct Reference

L2CAP packet structure. More...

Data Fields

uint16 CID
 local channel id More...
 
uint16 connHandle
 connection handle More...
 
uint16 len
 length of information payload More...
 
uint8 * pPayload
 

Detailed Description

L2CAP packet structure.

Field Documentation

§ CID

uint16 CID

local channel id

§ connHandle

uint16 connHandle

connection handle

§ len

uint16 len

length of information payload

§ pPayload

uint8* pPayload

pointer to information payload. This contains the payload received from the upper layer protocol (outgoing packet), or delivered to the upper layer protocol (incoming packet).


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale