TI BLE5-Stack API Documentation  9.14.01
Data Fields
l2capConnectReq_t Struct Reference

Connection Request format. More...

Data Fields

uint16 initCredits
 Indicates number of LE-frames that peer device can send. More...
 
uint16 mps
 
uint16 mtu
 
uint16 psm
 LE PSM. More...
 
uint16 srcCID
 Represents CID on device sending request and receiving response. More...
 

Detailed Description

Connection Request format.

Field Documentation

§ initCredits

uint16 initCredits

Indicates number of LE-frames that peer device can send.

§ mps

uint16 mps

Specifies Maximum PDU Payload Size (MPS) that can be received on this channel (Maximum Transmission Unit (MTU) for an outgoing/incoming L2CAP PDU.)

§ mtu

uint16 mtu

Specifies maximum SDU (service data unit) size that can be received on this channel (Maximum Transmission Unit for an unsegmented outgoing/incoming L2CAP SDU)

§ psm

uint16 psm

LE PSM.

§ srcCID

uint16 srcCID

Represents CID on device sending request and receiving response.


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale