TI BLE5-Stack API Documentation  9.14.01
Data Fields
hciEvt_NumCompletedPkt_t Struct Reference

Number of Completed Packets Event. More...

Data Fields

event_hdr_t hdr
 osal event header More...
 
uint8 numHandles
 number of handles More...
 
uint16 * pConnectionHandle
 pointer to the connection handle array More...
 
uint16 * pNumCompletedPackets
 pointer to the number of completed packets array More...
 

Detailed Description

Number of Completed Packets Event.

Field Documentation

§ hdr

osal event header

§ numHandles

uint8 numHandles

number of handles

§ pConnectionHandle

uint16* pConnectionHandle

pointer to the connection handle array

§ pNumCompletedPackets

uint16* pNumCompletedPackets

pointer to the number of completed packets array


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale