![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.01
|
LE Data Length Change Event. More...
Data Fields | |
| uint8 | BLEEventCode |
| BLE Event Code. More... | |
| uint16 | connHandle |
| connection handle More... | |
| event_hdr_t | hdr |
| osal event header More... | |
| uint16 | maxRxOctets |
| maximum receive bytes More... | |
| uint16 | maxRxTime |
| maximum receive time More... | |
| uint16 | maxTxOctets |
| maximum transmission bytes More... | |
| uint16 | maxTxTime |
| maximum transmission time More... | |
LE Data Length Change Event.
| uint8 BLEEventCode |
BLE Event Code.
| uint16 connHandle |
connection handle
| event_hdr_t hdr |
osal event header
| uint16 maxRxOctets |
maximum receive bytes
| uint16 maxRxTime |
maximum receive time
| uint16 maxTxOctets |
maximum transmission bytes
| uint16 maxTxTime |
maximum transmission time