TI BLE5-Stack API Documentation  9.14.01
Data Fields
CS_subeventResultsEvt_t Struct Reference

Data Fields

uint8_t abortReason
 abort reason CS_Abort_Reason More...
 
uint8_t configID
 configuration ID More...
 
uint16_t connHandle
 connection handle More...
 
csEventOpcodes_e csEvtOpcode
 CS Event Code csEventOpcodes_e. More...
 
uint8_t data []
 Array of type csSubeventResultsStep_t. More...
 
uint16_t dataLen
 Data length. More...
 
int16_t frequencyCompensation
 frequency compensation More...
 
uint8_t numAntennaPath
 number of antenna paths More...
 
uint8_t numStepsReported
 number of steps reported More...
 
uint16_t procedureCounter
 procedure counter More...
 
uint8_t procedureDoneStatus
 procedure done status CS_Procedure_Done_Status More...
 
int8_t referencePowerLevel
 reference power level More...
 
uint16_t startAclConnectionEvent
 start ACL connection event More...
 
uint8_t subeventDoneStatus
 subevent done status More...
 

Field Documentation

§ abortReason

uint8_t abortReason

abort reason CS_Abort_Reason

§ configID

uint8_t configID

configuration ID

§ connHandle

uint16_t connHandle

connection handle

§ csEvtOpcode

csEventOpcodes_e csEvtOpcode

CS Event Code csEventOpcodes_e.

§ data

uint8_t data[]

Array of type csSubeventResultsStep_t.

§ dataLen

uint16_t dataLen

Data length.

§ frequencyCompensation

int16_t frequencyCompensation

frequency compensation

§ numAntennaPath

uint8_t numAntennaPath

number of antenna paths

§ numStepsReported

uint8_t numStepsReported

number of steps reported

§ procedureCounter

uint16_t procedureCounter

procedure counter

§ procedureDoneStatus

uint8_t procedureDoneStatus

procedure done status CS_Procedure_Done_Status

§ referencePowerLevel

int8_t referencePowerLevel

reference power level

§ startAclConnectionEvent

uint16_t startAclConnectionEvent

start ACL connection event

§ subeventDoneStatus

uint8_t subeventDoneStatus

subevent done status


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale