TI BLE5-Stack API Documentation  9.14.01
Data Fields
BLEAppUtil_AdvEventData_t Struct Reference

BLEAppUtil Adv Event Data Structure. More...

Data Fields

uint32_t * arg
 custom application argument that can be return through this callback More...
 
uint32_t event
 see BLEAppUtil_GAPAdvEventMaskFlags_e More...
 
GapAdv_data_tpBuf
 data potentially accompanying event More...
 

Detailed Description

BLEAppUtil Adv Event Data Structure.

Used to store the data of adv event

Field Documentation

§ arg

uint32_t* arg

custom application argument that can be return through this callback

§ event

uint32_t event

§ pBuf

data potentially accompanying event


The documentation for this struct was generated from the following file:
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale