![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.01
|
Modules | |
| GAP Bond Manager Callbacks | |
| GAP Bond Manager Constants | |
| GAP Bond Manager Pairing State Events | |
| GAP Bond Manager Parameters | |
| GAP Bond Manager Structures | |
Files | |
| file | gapbondmgr.h |
Functions | |
| bStatus_t | GAPBondMgr_FindAddr (uint8_t *pDevAddr, GAP_Peer_Addr_Types_t addrType, uint8_t *pIdx, GAP_Peer_Addr_Types_t *pIdentityAddrType, uint8_t *pIdentityAddr) |
| Search for an address in the bonding table. If the address is a random private resolvable address, attempt to resolve the random address against all IRK's in bonding table. As output parameters, return the following: More... | |
| bStatus_t | GAPBondMgr_GenerateEccKeys (void) |
| Generates ECC keys. More... | |
| uint8_t | GAPBondMgr_GetAuthTaskID (void) |
| Retrieves the Task ID associated with the GAP Bond Manager for authentication purposes. More... | |
| bStatus_t | GAPBondMgr_GetParameter (uint16_t param, void *pValue) |
| uint8_t | GapBondMgr_GetPrevAuth (uint16_t connHandle, uint8_t *pMitmReq, uint8_t *pKeySize) |
| bool | GAPBondMgr_isEnable (void) |
| bStatus_t | GAPBondMgr_Pair (uint16_t connHandle) |
| bStatus_t | GAPBondMgr_PasscodeRsp (uint16_t connectionHandle, uint8_t status, uint32_t passcode) |
| uint8_t | GapBondMgr_readBondFromNV (uint8_t mode, uint8_t *pIdentifier, GAP_Peer_Addr_Types_t addrType, gapBondNvRecord_t *pBondRecord) |
| void | GAPBondMgr_ReadCSRKFromNV (uint8_t *keyBuff) |
| Reads the stored CSRK (Connection Signature Resolving Key) from non-volatile memory into the provided buffer. More... | |
| void | GAPBondMgr_ReadIRKFromNV (uint8_t *keyBuff) |
| Reads the Identity Resolving Key (IRK) from non-volatile storage. More... | |
| bStatus_t | GAPBondMgr_ReadLocalLTK (GAP_Peer_Addr_Types_t addrType, uint8_t *pDevAddr, gapBondLTK_t *pLocalLtk) |
| void | GAPBondMgr_Register (gapBondCBs_t *pCB) |
| bStatus_t | GAPBondMgr_SCGetLocalOOBParameters (gapBondOOBData_t *localOobData) |
| Get local Random number and confirm value for secure connection. More... | |
| bStatus_t | GAPBondMgr_SCSetRemoteOOBParameters (gapBondOOBData_t *remoteOobData, uint8 OOBDataFlag) |
| Set remote's OOB parameters for secure connection. More... | |
| bStatus_t | GAPBondMgr_ServiceChangeInd (uint16_t connectionHandle, uint8_t setParam) |
| bStatus_t | GAPBondMgr_SetParameter (uint16_t param, uint8_t len, void *pValue) |
| uint8_t | GapBondMgr_StartEnc (uint16_t connHandle) |
| uint8_t | GapBondMgr_writeBondToNv (gapBondRec_t *pBondRec, gapBondLTK_t *pLocalLtk, gapBondLTK_t *pDevLtk, uint8_t *pIRK, uint8_t *pSRK, uint32_t signCount, gapBondCharCfg_t *charCfg) |
| Write bond record to NV. More... | |
This module implements the GAP Bond Manager
| bStatus_t GAPBondMgr_FindAddr | ( | uint8_t * | pDevAddr, |
| GAP_Peer_Addr_Types_t | addrType, | ||
| uint8_t * | pIdx, | ||
| GAP_Peer_Addr_Types_t * | pIdentityAddrType, | ||
| uint8_t * | pIdentityAddr | ||
| ) |
Search for an address in the bonding table. If the address is a random private resolvable address, attempt to resolve the random address against all IRK's in bonding table. As output parameters, return the following:
Note that the output parameters are optional. If it is not desired for them to be returned, a NULL pointer can safely be passed.
| pDevAddr | peer's address |
| addrType | peer's address type |
| pIdx | pointer to byte to put the bond index if found |
| pIdentityAddrType | pointer to byte to put the identity address type if applicable |
| pIdentityAddr | pointer to buffer to put the identity address type if applicable |
| bStatus_t GAPBondMgr_GenerateEccKeys | ( | void | ) |
Generates ECC keys.
/ref did_244389729
| uint8_t GAPBondMgr_GetAuthTaskID | ( | void | ) |
Retrieves the Task ID associated with the GAP Bond Manager for authentication purposes.
This function returns the Task ID that is used by the GAP Bond Manager to handle authentication-related events and operations. It is typically used internally within the BLE stack to manage bonding and security tasks.
| bStatus_t GAPBondMgr_GetParameter | ( | uint16_t | param, |
| void * | pValue | ||
| ) |
Get a GAP Bond Manager parameter.
| param | Profile parameter ID: GAP Bond Manager Parameters |
| pValue | pointer to location to get the value. This is dependent on the parameter ID and WILL be cast to the appropriate data type (example: data type of uint16_t will be cast to uint16_t pointer). |
| uint8_t GapBondMgr_GetPrevAuth | ( | uint16_t | connHandle, |
| uint8_t * | pMitmReq, | ||
| uint8_t * | pKeySize | ||
| ) |
| bool GAPBondMgr_isEnable | ( | void | ) |
| bStatus_t GAPBondMgr_Pair | ( | uint16_t | connHandle | ) |
Start (or re-start) the pairing process
This API can be used to initiate pairing in cases where it is not started automatically by the gapbondmgr or to re-pair after the initial pairing has occurred if, for example, the pairing requirements have changed.
| connHandle | connection handle to initiate pairing with |
| bStatus_t GAPBondMgr_PasscodeRsp | ( | uint16_t | connectionHandle, |
| uint8_t | status, | ||
| uint32_t | passcode | ||
| ) |
Respond to a passcode request.
| connectionHandle | connection handle of the connected device or 0xFFFF if all devices in database. |
| status | SUCCESS if passcode is available, otherwise see Pairing failure status values. |
| passcode | integer value containing the passcode. |
| uint8_t GapBondMgr_readBondFromNV | ( | uint8_t | mode, |
| uint8_t * | pIdentifier, | ||
| GAP_Peer_Addr_Types_t | addrType, | ||
| gapBondNvRecord_t * | pBondRecord | ||
| ) |
| void GAPBondMgr_ReadCSRKFromNV | ( | uint8_t * | keyBuff | ) |
Reads the stored CSRK (Connection Signature Resolving Key) from non-volatile memory into the provided buffer.
| keyBuff | Pointer to a buffer where the CSRK will be copied. The buffer must be large enough to hold the CSRK. |
| void GAPBondMgr_ReadIRKFromNV | ( | uint8_t * | keyBuff | ) |
Reads the Identity Resolving Key (IRK) from non-volatile storage.
This function retrieves the IRK, which is used for resolving private addresses in Bluetooth Low Energy (BLE) communication, and stores it in the provided buffer.
| [out] | keyBuff | Pointer to a buffer where the IRK will be stored. The buffer must be large enough to hold the IRK (typically 16 bytes). |
| bStatus_t GAPBondMgr_ReadLocalLTK | ( | GAP_Peer_Addr_Types_t | addrType, |
| uint8_t * | pDevAddr, | ||
| gapBondLTK_t * | pLocalLtk | ||
| ) |
| void GAPBondMgr_Register | ( | gapBondCBs_t * | pCB | ) |
Register callback functions with the bond manager.
| pCB | pointer to callback function structure. |
| bStatus_t GAPBondMgr_SCGetLocalOOBParameters | ( | gapBondOOBData_t * | localOobData | ) |
Get local Random number and confirm value for secure connection.
/ref did_244389729
| localOobData | - Struct holding local's random number and confirm value |
| bStatus_t GAPBondMgr_SCSetRemoteOOBParameters | ( | gapBondOOBData_t * | remoteOobData, |
| uint8 | OOBDataFlag | ||
| ) |
Set remote's OOB parameters for secure connection.
/ref did_244389729
| remoteOobData | - struct holding remote random number and confirm value |
| OOBDataFlag | - 1 - OOB Authentication data from remote device present, else 0 |
| bStatus_t GAPBondMgr_ServiceChangeInd | ( | uint16_t | connectionHandle, |
| uint8_t | setParam | ||
| ) |
Set/clear the service change indication in a bond record.
| connectionHandle | connection handle of the connected device or 0xFFFF if all devices in database. |
| setParam | TRUE to set the service change indication, FALSE to clear it. |
| bStatus_t GAPBondMgr_SetParameter | ( | uint16_t | param, |
| uint8_t | len, | ||
| void * | pValue | ||
| ) |
Set a GAP Bond Manager parameter.
| param | GAP Bond Manager Parameters |
| len | length of data to write |
| pValue | pointer to data to write. This is dependent on the parameter ID and WILL be cast to the appropriate data type (example: data type of uint16_t will be cast to uint16_t pointer). |
| uint8_t GapBondMgr_StartEnc | ( | uint16_t | connHandle | ) |
| uint8_t GapBondMgr_writeBondToNv | ( | gapBondRec_t * | pBondRec, |
| gapBondLTK_t * | pLocalLtk, | ||
| gapBondLTK_t * | pDevLtk, | ||
| uint8_t * | pIRK, | ||
| uint8_t * | pSRK, | ||
| uint32_t | signCount, | ||
| gapBondCharCfg_t * | charCfg | ||
| ) |
Write bond record to NV.
| pBondRec | - basic bond record |
| pLocalLTK | - LTK used by the device that has the same public address as current device |
| pDevLTK | - LTK used by the peer device during pairing |
| pIRK | - IRK used by the peer device during pairing |
| pSRK | - SRK used by the peer device during pairing |
| signCounter | - Sign counter used by the peer device during pairing |
| charCfg | - GATT characteristic configuration |