![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.01
|
GAP layer parameters
| enum Gap_configParamIds_t |
GAP Configuration Parameters
These can be set with GapConfig_SetParameter
| Enumerator | |
|---|---|
| GAP_CONFIG_PARAM_IRK | Can be used by the application to set the IRK. It is not necessary to set this parameter. If it is not set, a random IRK will be generated unless there is a valid IRK in NV.
The priority is:
size: 16 bytes
|
| GAP_CONFIG_PARAM_SRK | Can be used by the application to set the SRK. It is not necessary to set this parameter. If it is not set, a random SRK will be generated unless there is a valid SRK in NV.
The priority is:
size: 16 bytes
|
| GAP_CONFIG_PARAM_IRK_UPDATE_IMMED | Can be used by the application to update the IRK immediately. It is not necessary to set this parameter. If it is not set, a random IRK will be generated unless there is a valid IRK in NV.
size: 16 bytes
|
| enum Gap_ParamIDs_t |
GAP Parameter IDs
Parameters set via GAP_SetParamValue
| Enumerator | |
|---|---|
| GAP_PARAM_LINK_UPDATE_DECISION | Action to take upon receiving a parameter update request. default: GAP_UPDATE_REQ_PASS_TO_APP range: Gap_updateDecision_t |
| GAP_PARAM_CONN_PARAM_TIMEOUT | Connection Parameter timeout. Minimum time after an L2CAP Connection Parameter Update Response has been received that a L2CAP Connection Parameter Update Request can be sent. See section Version 5.0 Vol 3, Part C, Section 9.3.9.2 of the BT Core Spec default: 30000 range: 1-65535 |
| GAP_PARAM_PRIVATE_ADDR_INT | Minimum Time Interval between private (resolvable) address changes (minutes)
default: 15 range: 1-65535 |
| GAP_PARAM_SM_TIMEOUT | Time to wait for security manager response before returning bleTimeout (ms) default: 30000 range: 1-65535 |
| GAP_PARAM_SM_MIN_KEY_LEN | SM Minimum Key Length supported default: 7 range: 1-65535 |
| GAP_PARAM_SM_MAX_KEY_LEN | SM Maximum Key Length supported default: 16 range: 1-65535 |