TI BLE5-Stack API Documentation  9.14.01
Data Structures
BLEAppUtil Structures

This module implements BLEAppUtil structures. More...

Data Structures

struct  BLEAppUtil_AdvEventData_t
 BLEAppUtil Adv Event Data Structure. More...
 
struct  BLEAppUtil_AdvInit_t
 BLEAppUtil Adv Init Structure. More...
 
struct  BLEAppUtil_AdvStart_t
 BLEAppUtil Adv Start Structure. More...
 
struct  BLEAppUtil_ConnectParams_t
 BLEAppUtil Connect Params Structure. Should be created by the application and passed to BLEAppUtil_Connect. More...
 
struct  BLEAppUtil_ConnParams_t
 BLEAppUtil Conn Params Structure. Should be created by the application and passed to BLEAppUtil_setConnParams. More...
 
struct  BLEAppUtil_ConnPhyParams_t
 Phy Preference on the current connection. Should be created by the application and passed to BLEAppUtil_setConnPhy. More...
 
struct  BLEAppUtil_EventHandler_t
 BLEAppUtil Events handlers Structure. More...
 
struct  BLEAppUtil_GapScan_Evt_AdvRpt_t
 
struct  BLEAppUtil_GeneralParams_t
 BLEAppUtil General Params Structure. More...
 
struct  BLEAppUtil_PairStateData_t
 BLEAppUtil PairState Event Data Structure. More...
 
struct  BLEAppUtil_PasscodeData_t
 BLEAppUtil Passcode Data Structure. More...
 
struct  BLEAppUtil_PeriCentParams_t
 BLEAppUtil Peripheral Central Params Structure. More...
 
struct  BLEAppUtil_ScanEventData_t
 BLEAppUtil Scan Event Data Structure. More...
 
struct  BLEAppUtil_ScanInit_t
 BLEAppUtil Scan Init Structure. More...
 
struct  BLEAppUtil_ScanStart_t
 BLEAppUtil Scan Start Structure. More...
 
union  GapAdv_data_t
 
union  GapScan_data_t
 

Detailed Description

This module implements BLEAppUtil structures.

© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale