![]() |
![]() |
|
TI BLE5-Stack API Documentation
9.14.01
|
This module implements BLEAppUtil Functions Typedefs. More...
Typedefs | |
| typedef uint8_t | BLEAppUtil_BDaddr[B_ADDR_LEN] |
| Device Address. More... | |
| typedef ICall_Hdr | BLEAppUtil_msgHdr_t |
| typedef void(* | EventHandler_t) (uint32 event, BLEAppUtil_msgHdr_t *pMsgData) |
| Event handler which used in BLEAppUtil_EventHandler_t. More... | |
| typedef void(* | InvokeFromBLEAppUtilContext_t) (char *pData) |
| Profile/Service Invoke from BLE App Util context type. This callback is used by BLEAppUtil_invokeFunction and BLEAppUtil_invokeFunctionNoData. More... | |
| typedef void(* | StackInitDone_t) (gapDeviceInitDoneEvent_t *deviceInitDoneData) |
| A callback which will be called when Device Initialization Done event is raised. Should be sent to BLEAppUtil_init. More... | |
This module implements BLEAppUtil Functions Typedefs.
| typedef uint8_t BLEAppUtil_BDaddr[B_ADDR_LEN] |
Device Address.
| typedef ICall_Hdr BLEAppUtil_msgHdr_t |
| typedef void(* EventHandler_t) (uint32 event, BLEAppUtil_msgHdr_t *pMsgData) |
Event handler which used in BLEAppUtil_EventHandler_t.
| event | - message event. |
| pMsgData | - pointer to message data. |
| typedef void(* InvokeFromBLEAppUtilContext_t) (char *pData) |
Profile/Service Invoke from BLE App Util context type. This callback is used by BLEAppUtil_invokeFunction and BLEAppUtil_invokeFunctionNoData.
| pData | - The data to provide the callback |
| typedef void(* StackInitDone_t) (gapDeviceInitDoneEvent_t *deviceInitDoneData) |
A callback which will be called when Device Initialization Done event is raised. Should be sent to BLEAppUtil_init.
| deviceInitDoneData | - Init Done data which shall be used by the callback. the data is of the format: gapDeviceInitDoneEvent_t. |