TI BLE5-Stack API Documentation  9.14.01
comdef.h
Go to the documentation of this file.
1 /******************************************************************************
2 
3  @file comdef.h
4 
5  @brief This file contains useful macros and data types
6 
7  Group: WCS, LPC, BTS
8  $Target Device: DEVICES $
9 
10  ******************************************************************************
11  $License: BSD3 2004 $
12  ******************************************************************************
13  $Release Name: PACKAGE NAME $
14  $Release Date: PACKAGE RELEASE DATE $
15  *****************************************************************************/
16 
22 #ifndef COMDEF_H
23 #define COMDEF_H
24 
25 #ifdef __cplusplus
26 extern "C"
27 {
28 #endif
29 
30 
31 /*********************************************************************
32  * INCLUDES
33  */
34 
35 #include <stdint.h>
36 #include <stdbool.h>
37 
39 
40 /*********************************************************************
41  * Lint Keywords
42  */
43 #define VOID (void)
44 
45 /*********************************************************************
46  * CONSTANTS
47  */
48 
49 #ifndef false
50  #define false 0
51 #endif
52 
53 #ifndef true
54  #define true 1
55 #endif
56 
57 #ifndef GENERIC
58  #define GENERIC
59 #endif
60 
61 #ifndef TRUE
62 #define TRUE 1
63 #endif
64 
65 #ifndef UTRUE
66 #define UTRUE 1U
67 #endif
68 
69 #ifndef FALSE
70 #define FALSE 0
71 #endif
72 
73 #ifndef UFALSE
74 #define UFALSE 0U
75 #endif
76 
77 // Fix to stdint.h definitions
78 #ifdef UINT8_MAX
79 #undef UINT8_MAX
80 #define UINT8_MAX 255U
81 #endif
82 
83 #ifdef UINT16_MAX
84 #undef UINT16_MAX
85 #define UINT16_MAX 65535U
86 #endif
87 
89 
90 /*** Generic Status Return Values ***/
91 #define SUCCESS 0x00
92 #define USUCCESS 0U
93 #define FAILURE 0x01
94 #define UFAILURE 1U
95 #define INVALIDPARAMETER 0x02
96 #define UINVALIDPARAMETER 2U
97 #define INVALID_TASK 0x03
98 #define MSG_BUFFER_NOT_AVAIL 0x04
99 #define INVALID_MSG_POINTER 0x05
100 #define INVALID_EVENT_ID 0x06
101 #define INVALID_INTERRUPT_ID 0x07
102 #define NO_TIMER_AVAIL 0x08
103 #define NV_ITEM_UNINIT 0x09
104 #define NV_OPER_FAILED 0x0A
105 #define INVALID_MEM_SIZE 0x0B
106 #define NV_BAD_ITEM_LEN 0x0C
107 
108 /*********************************************************************
109  * TYPEDEFS
110  */
111 
113 
114 // Generic Status return
115 typedef uint8_t Status_t;
116 
117 // Data types
118 typedef signed char int8;
119 typedef unsigned char uint8;
120 
121 typedef signed short int16;
122 typedef unsigned short uint16;
123 
124 typedef signed long int32;
125 typedef unsigned long uint32;
126 
127 typedef uint32_t halDataAlign_t;
128 
130 
131 /*********************************************************************
132  * MACROS
133  */
134 
135 #ifndef BV
136 #define BV(n) (1 << (n))
137 #endif
138 
139 #ifndef BF
140 #define BF(x,b,s) (((x) & (b)) >> (s))
141 #endif
142 
143 #ifndef ABS
144 #define ABS(n) (((n) < 0) ? -(n) : (n))
145 #endif
146 
147 // Break a uint32_t variable into a specific byte
148 #define BREAK_UINT32(var, ByteNum) \
149  ((((var) >> ((ByteNum) * 8)) & 0x00FF))
150 
151 // Build a uint32_t from four bytes
152 #define BUILD_UINT32(Byte0, Byte1, Byte2, Byte3) ( (((Byte3) & 0xFF) << 24) | \
153  (((Byte2) & 0xFF) << 16) | \
154  (((Byte1) & 0xFF) << 8) | \
155  ((Byte0) & 0xFF) )
156 
157 // Build a uint16_t from two bytes
158 #define BUILD_UINT16(loByte, hiByte) ( ((loByte) & 0xFF) | (((hiByte) & 0xFF) << 8) )
159 
160 // Get the high byte of a uint16_t
161 #define HI_UINT16(a) (((a) >> 8) & 0xFF)
162 
163 // Get the low byte of a uint16_t
164 #define LO_UINT16(a) ((a) & 0xFF)
165 
166 // Get a uint16_t from a pointer to a byte array
167 #define GET_UINT16(a) ((uint16_t)((*((uint8_t *)a)) + (((uint16_t)(*(((uint8_t *)a) + 1))) << 8)))
168 
169 // Build a uint8_t from two nibbles
170 #define BUILD_UINT8(hiByte, loByte) \
171  (((loByte) & 0x0F) + (((hiByte) & 0x0F) << 4))
172 
173 // Get the high nibble of a uint8_t
174 #define HI_UINT8(a) (((a) >> 4) & 0x0F)
175 
176 // Get the low nibble of a uint8_t
177 #define LO_UINT8(a) ((a) & 0x0F)
178 
179 // Write the 32bit value of 'val' in little endian format to the buffer pointed
180 // to by pBuf, and increment pBuf by 4
181 #define UINT32_TO_BUF_LITTLE_ENDIAN(pBuf, val) \
182  do { \
183  *(pBuf)++ = ((val >> 0) & 0xFF); \
184  *(pBuf)++ = ((val >> 8) & 0xFF); \
185  *(pBuf)++ = ((val >> 16) & 0xFF); \
186  *(pBuf)++ = ((val >> 24) & 0xFF); \
187  } while (0)
188 
189 // Return the 32bit little-endian formatted value pointed to by pBuf, and increment pBuf by 4
190 #define BUF_TO_UINT32_LITTLE_ENDIAN(pBuf) (((pBuf) += 4), BUILD_UINT32((pBuf)[-1], (pBuf)[-2], (pBuf)[-3], (pBuf)[-4]))
191 
192 #ifndef GET_BIT
193 // Macro to get the value of a specific bit in a byte array
194 #define GET_BIT(DISCS, IDX) (((DISCS)[((IDX) / 8)] & BV((IDX) % 8)) ? TRUE : FALSE)
195 #endif
196 
197 #ifndef SET_BIT
198 // Macro to set a specific bit in a byte array
199 #define SET_BIT(DISCS, IDX) (((DISCS)[((IDX) / 8)] |= BV((IDX) % 8)))
200 #endif
201 
202 #ifndef CLR_BIT
203 // Macro to clear a specific bit in a byte array
204 #define CLR_BIT(DISCS, IDX) (((DISCS)[((IDX) / 8)] &= (BV((IDX) % 8) ^ 0xFF)))
205 #endif
206 
207 /*
208  * This macro is for use by other macros to form a fully valid C statement.
209  * Without this, the if/else conditionals could show unexpected behavior.
210  *
211  * For example, use...
212  * #define SET_REGS() st( ioreg1 = 0; ioreg2 = 0; )
213  * instead of ...
214  * #define SET_REGS() { ioreg1 = 0; ioreg2 = 0; }
215  * or
216  * #define SET_REGS() ioreg1 = 0; ioreg2 = 0;
217  * The last macro would not behave as expected in the if/else construct.
218  * The second to last macro will cause a compiler error in certain uses
219  * of if/else construct
220  *
221  * It is not necessary, or recommended, to use this macro where there is
222  * already a valid C statement. For example, the following is redundant...
223  * #define CALL_FUNC() st( func(); )
224  * This should simply be...
225  * #define CALL_FUNC() func()
226  *
227  * (The while condition below evaluates false without generating a
228  * constant-controlling-loop type of warning on most compilers.)
229  */
230 #define st(x) do { x } while (__LINE__ == -1)
231 
232 /*
233  * The offsetof macro is a standard macro defined in the C standard library header <stddef.h>
234  * It is used to determine the byte offset of a member within a structure type.
235  */
236 #ifndef offsetof
237 #define offsetof(TYPE, MEMBER) ((size_t) &((TYPE *)0)->MEMBER)
238 #endif
239 /*********************************************************************
240  * MEMORY ATTRIBUTES
241  */
242 
243 #if defined (__IAR_SYSTEMS_ICC__)
244 #define XDATA
245 #define CODE
246 #define DATA_ALIGN(x) _Pragma data_alignment=(x)
247 #define ALIGNED
248 #define PACKED __packed
249 #define PACKED_STRUCT PACKED struct
250 #define PACKED_TYPEDEF_STRUCT PACKED typedef struct
251 #define PACKED_TYPEDEF_CONST_STRUCT PACKED typedef const struct
252 #define PACKED_TYPEDEF_UNION PACKED typedef union
253 #define PACKED_ALIGNED PACKED
254 #define PACKED_ALIGNED_TYPEDEF_STRUCT PACKED_TYPEDEF_STRUCT
255 
256 #elif defined __TI_COMPILER_VERSION || defined __TI_COMPILER_VERSION__
257 #define XDATA
258 #define CODE
259 #define DATA
260 #define NEARFUNC
261 #define ALIGNED
262 #define PACKED __attribute__((packed))
263 #define PACKED_STRUCT struct PACKED
264 #define PACKED_TYPEDEF_STRUCT typedef struct PACKED
265 #define PACKED_TYPEDEF_CONST_STRUCT typedef const struct PACKED
266 #define PACKED_TYPEDEF_UNION typedef union PACKED
267 #define PACKED_ALIGNED __attribute__((packed,aligned(4)))
268 #define PACKED_ALIGNED_TYPEDEF_STRUCT typedef struct PACKED_ALIGNED
269 
270 #elif defined (__GNUC__)
271 #define ALIGNED __attribute__((aligned(4)))
272 #ifdef CC33xx
273 #define PACKED __attribute__((aligned(1))) __attribute__((packed))
274 #else
275 #define PACKED __attribute__((__packed__))
276 #endif
277 #define PACKED_STRUCT struct PACKED
278 #define PACKED_TYPEDEF_STRUCT typedef struct PACKED
279 #define PACKED_TYPEDEF_CONST_STRUCT typedef const struct PACKED
280 #define PACKED_TYPEDEF_UNION typedef union PACKED
281 #define PACKED_ALIGNED __attribute__((packed,aligned(4)))
282 #define PACKED_ALIGNED_TYPEDEF_STRUCT typedef struct PACKED_ALIGNED
283 #endif
284 
285 /*********************************************************************
286  * COMPILER MACROS
287  */
288 
289 /* ----------- IAR Compiler ----------- */
290 #ifdef __IAR_SYSTEMS_ICC__
291 #define ASM_NOP asm("NOP")
292 #define NO_INIT __no_init
293 #define WEAK_FUNC __weak
294 
295 /* ----------- KEIL Compiler ----------- */
296 #elif defined __KEIL__
297 #define ASM_NOP __nop()
298 
299 /* ----------- CCS Compiler ----------- */
300 #elif defined __TI_COMPILER_VERSION || defined __TI_COMPILER_VERSION__
301 #define ASM_NOP asm(" NOP")
302 #define NO_INIT __attribute__((noinit))
303 
304 /* ----------- GNU Compiler ----------- */
305 #elif defined __GNUC__
306 #define ASM_NOP __asm__ __volatile__ ("nop")
307 #define WEAK_FUNC __attribute__((__weak__))
308 
309 /* ---------- MSVC compiler ---------- */
310 #elif _MSC_VER
311 #define ASM_NOP __asm NOP
312 
313 /* ----------- Unrecognized Compiler ----------- */
314 #else
315 #error "ERROR: Unknown compiler."
316 #endif
317 
318 /*********************************************************************
319  * GLOBAL VARIABLES
320  */
321 
322 /*********************************************************************
323  * FUNCTIONS
324  */
325 
326 /*********************************************************************
327 *********************************************************************/
328 
329 #ifdef __cplusplus
330 }
331 #endif
332 
333 #endif /* COMDEF_H */
© Copyright 1995-2025, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale