Example Summary
This example shows how to enable exception decoding.
Peripherals & Pin Assignments
When this project is built, the SysConfig tool will generate the TI-Driver configurations into the ti_drivers_config.c and ti_drivers_config.h files. Information on pins and resources used is present in both generated files. Additionally, the System Configuration file (*.syscfg) present in the project may be opened with SysConfig’s graphical user interface to determine pins and resources used.
CONFIG_GPIO_LED_0- GPIO instance used to control the onboard LED.
BoosterPacks, Board Resources & Jumper Settings
For board specific jumper settings, resources and BoosterPack modifications, refer to the Board.html file.
If you’re using an IDE such as Code Composer Studio (CCS) or IAR, please refer to Board.html in your project directory for resources used and board-specific jumper settings.
The Board.html can also be found in your SDK installation:
<SDK_INSTALL_DIR>/source/ti/boards/<BOARD>
Example Usage
After the device is powered on, a fault will be generated. CONFIG_GPIO_LED_0 should now be turned on.
If you are using the default log sink, LogSinkBuf, you can read out the log messages generated using ROV.
If you decide to change the default log sink, you should launch the tilogger python tool. For installation and usage of the tool see:
<SDK_INSTALL_DIR>/tools/log/tiutils/README.html
Application Design Details
The example will attempt to make a function call at an illegal address. That will trigger a fault.
The exception handler used, Exception_handlerMax(), will:
- Disable interrupts.
- Save the CPU state when the exception occurred.
- Decode the exception.
- Log the exception cause.
- Log the exception CPU state when the exception occurred.
- Log all Arm Cortex-M debug registers.
- Call the application’s implementation of
Exception_hookFxn(). - Spin in place.
Exception_hookFxn() will check the program counter of the Exception_ExceptionContext to see that it matches the expected illegal address. If they match, the function will turn on CONFIG_GPIO_LED_0. This is meant only to demonstrate how to access the CPU register state from the hook function. In a real application, this might be replaced by saving critical state in flash or other storage before gracefully resetting the device.
FreeRTOS:
- Please view the
FreeRTOSConfig.hheader file for example configuration information.