Basic BLE Profiles Project
Table of Contents
Introduction
The Basic BLE Profiles project is based on the Basic BLE example and implements a simple Bluetooth low-energy peripheral device with GATT profiles.
This project can be a framework for developing many different peripheral-role applications.
Hardware Prerequisites
The default Basic BLE Profiles board configuration uses the
device's LaunchPad development kit.
Software Prerequisites
For information on what versions of Code Composer Studio and IAR Embedded Workbench to use, see the Release Notes file provided in the SDK. In addition, please refer to the User's Guide for information on importing this project into your IDE workspace and build/run.
GATT Profiles
The GATT profiles can be configured using The "Profiles Configuration" option in SysConfig located within the BLE stack module.
Device Info
The Device Info Service is based on version 1.1 of BT SIG, exposes manufacturer and/or vendor information about a device.
Service Table
| Description | UUID | Format | Properties |
|---|---|---|---|
| Device Information Service | 180A | _Service declaration_ | Read |
| System ID | 2A23 | 8 bytes uint8 | Read |
| Model Number | 2A24 | 21 bytes uint8 | Read |
| Serial Number | 2A25 | 21 bytes uint8 | Read |
| Firmware Revision | 2A26 | 21 bytes uint8 | Read |
| Hardware Revision | 2A27 | 21 bytes uint8 | Read |
| Software Revision | 2A28 | 21 bytes uint8 | Read |
| Manufacturer Name | 2A29 | 21 bytes uint8 | Read |
| IEEE Regulatory Certification | 2A2A | The length of this characteristic is not fixed | Read |
| PnP ID | 2A50 | 7 bytes uint8 | Read |
Simple GATT
The Simple GATT profile is an example of a non BT SIG profile. It demonstrates various types of characteristics, permissions, and properties.
Service Table
| Description | UUID | Format | Properties |
|---|---|---|---|
| Simple GATT Service | F000FFF0-0451-4000-B000-000000000000 | _Service declaration_ | Read |
| Characteristic 1 | F000FFF1-0451-4000-B000-000000000000 | 1 byte uint8 | Read / Write |
| Characteristic 2 | F000FFF2-0451-4000-B000-000000000000 | 1 byte uint8 | Read |
| Characteristic 3 | F000FFF3-0451-4000-B000-000000000000 | 1 byte uint8 | Write |
| Characteristic 4 | F000FFF4-0451-4000-B000-000000000000 | 1 byte uint8 | Read / Write / Notify |
| Characteristic 5 | F000FFF5-0451-4000-B000-000000000000 | 5 bytes uint8 | Read (Authentication required) |
Continuous Glucose Monitoring
The Continuous Glucose Monitoring (CGM) profile, based on version 1.0.2 of BT SIG. It connects to a Central device and generates dummy glucose measurement values.
Service Table
| Description | UUID | Format | Properties |
|---|---|---|---|
| CGM Service | 181F | _Service declaration_ | Read |
| CGM Measurement | 2AA7 | 1 byte uint8 | Read / Write / Notify (Authentication required) |
| CGM Feature | 2AA8 | 4 bytes uint8 | Read (Authentication required) |
| CGM Status | 2AA9 | 3 bytes uint8 | Read (Authentication required) |
| CGM Session Start Time | 2AAA | 9 bytes uint8 | Read / Write (Authentication required) |
| CGM Session Run Time | 2AAB | 2 bytes uint8 | Read (Authentication required) |
| Record Access Control Point | 2A52 | 2-20 bytes uint8 | Read / Write / Indicate (Authentication required) |
| CGM Specific Ops Control Point | 2AAC | 1-18 bytes uint8 | Read / Write / Indicate (Authentication required) |
Glucose
Once the Glucose (GLS) profile, based on version 1.0.1 of BT SIG, connects to a Central device, it generates dummy glucose measurement values.
Service Table
| Description | UUID | Format | Properties |
|---|---|---|---|
| GLS Service | 1808 | _Service declaration_ | Read |
| GLS Measurement | 2A18 | 1 byte uint8 | Notify |
| GLS Feature | 2A51 | 2 bytes uint16 | Read (Authentication required) |
| Record Access Control Point | 2A52 | 2-20 bytes uint8 | Read / Write / Indicate (Authentication required) |
Health Thermometer
Once the Health Thermometer (HT) profile, based on version 1.0 of BT SIG, connects to a Central device, it generates dummy glucose measurement values.
Service Table
| Description | UUID | Format | Properties |
|---|---|---|---|
| HT Service | 1809 | _Service declaration_ | Read |
| HT Measurement | 2A1C | 1 byte uint8 | Read / Write / Indicate |
Battery Service
Once the Battery (BA) profile, based on version 1.1 of BT SIG, connects to a Central device, it updates the battery level every one minute and sends a notification over GATT notification.
Service Table
| Description | UUID | Format | Properties |
|---|---|---|---|
| BA Service | 180F | _Service declaration_ | Read |
| BA Level | 2A19 | 1 byte uint8 | Read / Notify |
Usage
To interact with the application over Bluetooth, you may use any device that can act as a BLE Central device, such as
iOS with the apps SimpleLink Connect or other BLE application
Android with the apps SimpleLink Connect or other BLE application
A CC26xx/CC13xx/CC23xx LaunchPad running the sample app HostTest from a compatible SDK with the PC tool BTool from the same SDK.
UART
This application uses the UART peripheral to provide an interface for the application. The UART is only used for display messages.
We recommend using a terminal program that can parse ANSI/VT100 color codes, such as Tera Term, PuTTY, Code Composer Studio Terminal, etc., to monitor the LaunchPad UART output.
The following default parameters are used for the UART peripheral for display:
| UART Param | Default Values |
|---|---|
| Baud Rate | 115200 |
| Data length | 8 bits |
| Parity | None |
| Stop bits | 1 bit |
| Flow Control | None |