Example Summary
This example performs raw read and write operations with a Secure Digital (SD) card. This example may corrupt any file system present on a SD card.
Peripherals & Pin Assignments
When this project is built, the SysConfig tool will generate the TI-Driver configurations into the ti_drivers_config.c and ti_drivers_config.h files. Information on pins and resources used is present in both generated files. Additionally, the System Configuration file (*.syscfg) present in the project may be opened with SysConfig’s graphical user interface to determine pins and resources used.
CONFIG_GPIO_LED_0- Indicates the SD card was successfully initialized.CONFIG_SD_0- SD driver instance.
BoosterPacks, Board Resources & Jumper Settings
This example requires a BOOSTXL-SHARP128 LCD & SD Card BoosterPack and a micro SD card.
For board specific jumper settings, resources and BoosterPack modifications, refer to the Board.html file.
If you’re using an IDE such as Code Composer Studio (CCS) or IAR, please refer to Board.html in your project directory for resources used and board-specific jumper settings.
The Board.html can also be found in your SDK installation:
<SDK_INSTALL_DIR>/source/ti/boards/<BOARD>
Example Usage
Example output is generated through use of Display driver APIs. Refer to the Display driver documentation.
- Open a serial session (e.g.
PuTTY, etc.) to the appropriate COM port.- The COM port can be determined via Device Manager in Windows or via
ls /dev/tty*in Linux.
- The COM port can be determined via Device Manager in Windows or via
The connection should have the following settings:
Baud-rate: 115200
Data bits: 8
Stop bits: 1
Parity: None
Flow Control: None
Edit the sdraw.c file and set WRITEENABLE to 1, and build the example. This will allow data to be written to the SD card. WARNING: Any file system present on the SD card will be overwritten and corrupted by this action!
Run the example.
CONFIG_GPIO_LED_0turns on to indicate successful driver initialization.The example reads and displays information about the SD card. An example is shown below:
======== SD Card Information ========
Sectors: 15196160
Sector Size: 512 bytes
Card Capacity: 7420 MB
=====================================
The example proceeds to write data to the SD card.
The example then reads back any data written.
The data read is compared with the data written. If they do not match, an error message will be displayed.
The data previously written is overwritten with 0.
If WRITEENABLE is 0, the example will only perform read operations.
Application Design Details
This application uses one thread:
The mainThread performs the following actions:
Create and initialize the SD driver.
Read the sector size and number of sectors from the SD card. This information is used to calculate the total card capacity.
Write raw data to the SD card.
Read data from the SD card and compare with data written.
The data previously written is erased by overwriting the data with 0.
FreeRTOS:
- Please view the
FreeRTOSConfig.hheader file for example configuration information.