GenMap

GenMap is a feature of SysConfig which allows for the generation of linker command file definitions (e.g. memory maps) and symbols suitable for inclusion in custom linker command files.

While GenMap is intentionally an optional feature, TI’s examples leverage it to improve their ability to migrate between devices, and remove hard-coded values that may otherwise require managing in multiple places.

Using GenMap linker definitions

SysConfig will now generate config- and device-related linker definitions in a new file named ti_utils_build_linker.cmd.genmap. This file will be created in the standard SysConfig output directory (e.g. {PROJECT_LOC}/{TARGET_CONFIGURATION}/syscfg when using CCS).

A user is able to include the ti_utils_build_linker.cmd.genmap in their application’s linker command file in order to reference the definitions within.

By default, the SDK examples include a linker file (with extension *.cmd for CCS, *.icf for IAR and *.ldf for GCC) which includes the ti_utils_build_linker.***.genmap file (where *** is the appropriate extension for the toolchain being used) and uses the definitions contained in the genmap.

The code snippet below shows how the genmap file may be included and how the definitions may be used in a linker file.

ti_utils_build_linker.cmd.genmap include and usage example
...
/* Including genmap file */
#include "ti_utils_build_linker.cmd.genmap"
...
/* Using genmap definitions in linker file */
#define FLASH_BASE              ti_utils_build_GenMap_FLASH0_BASE
#define FLASH_SIZE              ti_utils_build_GenMap_FLASH0_SIZE
#define RAM_BASE                ti_utils_build_GenMap_RAM0_BASE
#define RAM_SIZE                ti_utils_build_GenMap_RAM0_SIZE
...