SimpleLink™ CC23xx SDK Zigbee User's Guide
1.00.00
  • Introduction to the SimpleLink Low Power F3 SDK
  • Zigbee Quick Start Guide
  • Introduction
  • The CC23xx or CC27xx SDK Platform
  • FreeRTOS (RTOS Kernel) Overview
  • SimpleLink Low Power F3 SDK Overview
  • Developing Zigbee Applications
  • Developing with SimpleLink Low Power F3 SDK
  • MCUboot Over-the-Air Download (OAD)
  • Coexistence
  • Debugging
  • Packet Sniffer
  • System Configuration (SysConfig)
  • EnergyTrace User Guide
  • Migration Guide
  • References
SimpleLink™ CC23xx SDK Zigbee User's Guide
  • »
  • Segger J-Link support for CC1312PSIP in IAR

Segger J-Link support for CC1312PSIP in IAR¶

To be able to use a Segger J-Link probe with the CC1312PSIP in IAR, some configuration is required. Please configure the following in your IAR project settings.

Note

if IAR complains about the wrong CPU type, we need to modify the .ewp file which is located in the workspace of IAR as follows:


© Copyright 2005-2024, Texas Instruments.