Running Software Examples on the CC2755R10¶
Note
The software images built for CC23xx cannot be directly used on CC27xx. The software should be recompiled for CC27xx as described below.
Porting Software Examples for CC2755R10¶
The CC2755R10 is pin compatible with, and functionally identical to the CC2745R10-Q1 device for 2.4 GHz operation. You can run CC2745R10-Q1 software examples on the CC2755R10 device without making any changes.
Note
The also applies to the CC2745P10-Q1 in relation to CC2755P10 devices
Choosing LaunchPad for Development¶
The CC2745R10 LaunchPad is pin-to-pin compatible with CC2755R10 hardware. Therefore the on-board devices of these LaunchPads can be swapped for the desired CC2755R10 if specific hardware is not readily available. The correct example project must be selected for the specific device being used.
Moving From LaunchPad to Custom Board¶
You can find instructions on how to design and configure a custom board in the Custom Hardware chapter.