All notable changes to the ZBOSS stack are documented on this page.
ZBOSS 3.14.0.0 version dated 09/15/2022
This is a ZBOSS certification-ready release.
Improvement:
- [ZBS-392] - Add ability to trace binary string
- [ZBS-1016] - Improve zb_random() by using LFSR
- [ZBS-1166] - Move to use a device cb for the identify time attribute
- [ZBS-1187] - Add all possible baud rates to win_com_dump command options parser
- [ZBS-1188] - [GPCB] Implement GP Pairing Configuration with action = 0b101
- [ZBS-1205] - [GPCB] GP Pairing Configuration parsing is incomplete
- [ZBS-1257] - Improve GP accept commissioning handling
Tasks:
- [ZBS-256] - [NCP][Dump]Migrate to pcapng
- [ZBS-1120] - ZGPD build for nrf52833
- [ZBS-1255] - Deprecate ZGP_Match_Table
- [ZBS-1293] - [GPCB] Setup for testing 4.4.7.1/2/3 on the ZUTH
Bugs:
- [ZBS-86] - Packets are dropped from gpTxQueue after timeout in case of operational channel
- [ZBS-716] - lin_com_dump crashes when a platform has a symlink to the stack
- [ZBS-795] - Commissioning mode closed with Exit status
- [ZBS-799] - Fix GP cluster revision (4_3_10)
- [ZBS-808] - Bidirectional proximity commissioning: additional tests[4.4.1.7]
- [ZBS-1066] - [ZGP] Sink sends only IEEE part of frame during commissioning
- [ZBS-1099] - 4_3_4_4, 4_3_4_3 and 4_3_4_1 failed to get expected response to Add Group and Get Group Membership
- [ZBS-1108] - 4_4_7_2 and 4_4_7_3 failed on verifying sending or not sending Pairing
- [ZBS-1112] - 4_1_2_3 failed on the Read_Madatory_Attribute 0xfffd step
- [ZBS-1123] - 4_3_4_1_step_1 and 4_3_4_4 failed for several reasons
- [ZBS-1132] - Full device info removing in zb_nwk_ed_aging_timeout()
- [ZBS-1138] - 4_4_3_1 failed on the step GP Pairing
- [ZBS-1163] - 4_3_4_3 failed on several steps
- [ZBS-1165] - 4_4_1_13 failed on several steps
- [ZBS-1177] - 4_4_2_10_IAS_ZONE_step_1 failed on verification of sending GP Pairing
- [ZBS-1178] - 4_4_2_10_IAS_ZONE_step_3_6 failed on commissioning closing
- [ZBS-1179] - 4_4_2_10_NOTIAS_ZONE_step_1, step_2 failed on verification of sending GP Pairing
- [ZBS-1181] - 4_4_3_2 IAS_Zone and NOTIAS_Zone, 4_4_3_3, 4_4_3_4, 4_4_3_5. DUT GP Pairing responses on GP Pairing Configuration are incorrect
- [ZBS-1182] - Some ZCL command handlers do not send a default response if the command processing status is not OK.
- [ZBS-1189] - Invalid RSSI threshold value for zll
- [ZBS-1190] - Initiator asserts if target not found during touchlink scan
- [ZBS-1191] - Check a joining response status
- [ZBS-1196] - 4_4_1_12_step_9_14 failed on GP Pairing
- [ZBS-1198] - [GPCB] Fix GP cluster revision
- [ZBS-1200] - [GPCB] GPD_Channel_Configuration and GPD_Commissioning_Reply can not be sent
- [ZBS-1201] - [GPCB] ZB_APP_DESCR_TIMEOUT constant need to be aligned
- [ZBS-1202] - [GPCB] Add Groups and Level Control cluster to DUT (simple_combo(zc_combo.c))
- [ZBS-1229] - Empty frames on nrf52 platform with rx_on_when_idle=true
- [ZBS-1239] - [GPCB] Sink doesn't exit commissioning mode after Application Description timeout expired.
- [ZBS-1247] - Router rejoin failed
- [ZBS-1275] - [GPCB] Refactor sink table read attr logic, remove useless field
- [ZBS-1295] - [GPCB] Fix access to mapping table entries
- [ZBS-1311] - [GPCB] Fix GP Pairing Configuration with App description related bugs
ZBOSS 3.13.1.0 version dated 08/22/2022
This is a ZBOSS certification-ready release.
Improvement:
- [ZBS-1257] Improve GP accept commissioning handling (Done)
- [ZBS-1205] [GPCB] GP Pairing Configuration parsing is incomplete
- [ZBS-1187] Add all possible baud rates to win_com_dump command options parser
- [ZBS-1188] [GPCB] Implement GP Pairing Configuration with action = 0b101
- [ZBS-1016] Improve zb_random() by using LFSR
- [ZBS-1166] Move to use a device cb for the identify time attribute
Task:
- [ZBS-1120] ZGPD build for nrf52833
Bug:
- [ZBS-1198] [GPCB] Fix GP cluster revision
- [ZBS-1275] [GPCB] Refactor sink table read attr logic, remove useless field
- [ZBS-1201] [GPCB] ZB_APP_DESCR_TIMEOUT constant need to be aligned
- [ZBS-1182] Some ZCL command handlers do not send a default response if the command processing status is not OK.
- [ZBS-795] Commissioning mode closed with Exit status
- [ZBS-1229] Empty frames on nrf52 platform with rx_on_when_idle=true
- [ZBS-1202] [GPCB] Add Groups and Level Control cluster to DUT (simple_combo(zc_combo.c))
- [ZBS-1247] Router rejoin failed
- [ZBS-1239] [GPCB] Sink doesn't exit commissioning mode after Application Description timeout expired. (Done)
- [ZBS-1066] [ZGP] Sink sends only IEEE part of frame during commissioning
- [ZBS-1189] Invalid RSSI threshold value for zll
- [ZBS-1200] [GPCB] GPD_Channel_Configuration and GPD_Commissioning_Reply can not be sent
- [ZBS-1191] Check a joining response status (Done)
- [ZBS-1190] Initiator asserts if target not found during touchlink scan
ZBOSS 3.13.0.0 version dated 06/29/2022
This is a ZBOSS certification-ready release.
Tasks:
- [ZBS-255] [NCP][Dump]NCP dump for nsng build
- [ZBS-542] ZCL Manufacturer specific extensions support
- [ZBS-1036] ZCL OTA Cluster updates, fix some attributes requirements
- [ZBS-1062] FIx ZGPD development tool compilation
- [ZBS-250] [SECUR] backport to r22.2 r23 certification test 19.10 for Prevent rx-on-when-idle change on rejoin
- [ZBS-247] [SECUR] r22.2 test 19.11 for TC Rejoin in Distributed
Improvements:
- [ZBS-950] Unresolved dependencies in the NCP host shared library
- [ZBS-1032] win_com_dump does not decode Zephyr trace if Zephyr Shell is enabled.
- [ZBS-371] New sample: IC usage
- [ZBS-1022] ZGP Translation Table entry with 0xFF GPD command
- [ZBS-953] Possibility to change ZB_SCHED_SLEEP_NO_TM_BI value.
Bugfixes:
- [ZBS-1130] Fix certification tests compile for nRF52833 bm
- [ZBS-1033] win_com_dump: the logic for reading from standard input is broken.
- [ZBS-1156] [ZGP] Application description dataset unaligned to 4 bytes
- [ZBS-931] ZB_LS_SET_INCOMING_COST and?ZB_LS_SET_OUTGOING_COST macros are not resetting reserved bits
- [ZBS-1106] 4_4_2_17 and 4_4_2_18 DUT sends wrong GP response parameters
- [ZBS-1047] Fix issue with ZGP Sink Translation table iteration
- [ZBS-430] [ZCL] Don't execute general commands for MSP attributes with existing IDs
- [ZBS-1124] [ZGP] simple_combo sample is not working properly
- [ZBS-915] [ZUTH Testing][B-TC-02S] DeviceEnabled attribute not working
- [ZBS-911] Memory corruption in NCP_HL_GET_ZIGBEE_CHANNEL_MASK NCP command handler
- [ZBS-805] Bi-Directional commissioning issues [4.4.1.13, 4.4.1.14, 4.4.1.17, 4.4.1.19, 4.4.2.7]
- [ZBS-1071] Improper initialization of structure in ZB_ZCL_DECLARE_WAH_ATTRIB_LIST macro
- [ZBS-905] [ZCL8] Level Control Move to Level speed does not correspond to expected
- [ZBS-676] Get Group Membership Command returns all groups the node is assigned to
- [ZBS-1031] zb_nrf52_abort function needs to be "noreturn"
- [ZBS-1098] 5_4_1_2 failed on stepValidate_ZCL_Payload_of_GP_Commiss_Notif
- [ZBS-79] Poll interval changes not in zb_zdo_pim_set_long_poll_interval but on the next poll.
- [ZBS-221] Fix Clang warnings in stack.
- [ZBS-1109] 5_2_4_1 and 5_2_4_2 failed on steps validating ZCL Payload
- [ZBS-1114] set direction ZB_ZCL_FRAME_DIRECTION_TO_CLI
- [ZBS-205] [DOC] Old snippets from the non-public headers
- [ZBS-996] ZBOSS issue with Philips bulbs Mgmt leave
- [ZBS-963] Incorrect ZCL Default response on ZCL commands
- [ZBS-1080] Reduce error message trace level
- [ZBS-1103] 4_3_2 GPCB does not react on receiving GP Notification
- [ZBS-1105] 4_5_2_3 failed on steps Read_Mandatory_Attribute_0x0001
- [ZBS-1097] 5_3_1_6 failed on step Item_1d_Validate_ZCL_Payload
- [ZBS-1110] 5_3_1_2 and 5_3_1_3 failed on steps validating ZCL Payload
- [ZBS-1134] Fix default atributtes values for GP
- [ZBS-948] [NSNG] An overflow of the 32-bit signed integer leads to an incorrect 64-bit time value.
- [ZBS-1060] Application crashes using nrf52-bm platform with Hue bridge and bulbs
- [ZBS-806] Subsequent commissioning [4.4.1.15, 4.4.1.16, 4.4.1.20, 4.4.1.21, 4.4.2.13, 4.4.2.14]
- [ZBS-801] Failed on Step Item_P3_GP_Pairing_command (4_3_4_3, 4_3_9_2, 4_3_9_3)
Stories:
- [ZBS-698] Remove 'strange' words from code and comments
New Features:
- [ZBS-705] Getting serial port file descriptor for NCP transport
- [ZBS-797] Mapping table (optional but requested by customer): ZBS-232
- [ZBS-706] Function for getting time to next event for NCP
- [ZBS-232] [GP] Impossible to set endpoint for GPDF commands translation
- [ZBS-949] Trace output to stdout
ZBOSS 3.12.0.0 version dated 02/22/2022
This is a ZBOSS certification-ready release.
Tasks:
- [ZBS-527] [ZCL8] Problematic clusters from the backward compatibility point of view (check)
- [ZBS-684] [ZCL_BC] Command ZCL statuses parsing and aligning with currently used revision
- [ZBS-685] [ZCL_BC] Update send commands for Color Control cluster
- [ZBS-686] [ZCL_BC] Update send commands for Time cluster
- [ZBS-715] [ZCL_BC] Analyse per-cluster size change, which was caused by ZCL8+BC changes, optimize
- [ZBS-730] [ZCL_BC] Make aliases for all old functions and macroses which are used for SEND commands
- [ZBS-736] Implement ZB_VERIFY() macro
- [ZBS-779] ZR must send Update Device on receiving NWK LEAVE from other ZR
Improvements:
- [ZBS-263] [ZCL8][0x0000] Basic
- [ZBS-264] [ZCL8][0x0001] Power Configuration
- [ZBS-266] [ZCL8][0x0003] Identify
- [ZBS-267] [ZCL8][0x0004] Groups
- [ZBS-268] [ZCL8][0x0005] Scenes
- [ZBS-269] [ZCL8][0x0006] OnOff
- [ZBS-270] [ZCL8][0x0007] OnOff Switch Configuration
- [ZBS-271] [ZCL8][0x0008] Level (Base)
- [ZBS-272] [ZCL8][0x0009] Alarms
- [ZBS-273] [ZCL8][0x000a] Time
- [ZBS-276] [ZCL8][0x0b05] Diagnostics
- [ZBS-277] [ZCL8][0x0020] Poll Control
- [ZBS-279] [ZCL8][0x0025] Keep Alive
- [ZBS-282] [ZCL8][4][0x0400] Illuminance Measurement
- [ZBS-284] [ZCL8][4][0x0402] Temperature Measurement
- [ZBS-285] [ZCL8][4][0x0403] Pressure Measurement
- [ZBS-287] [ZCL8][4][0x0405] Water Content Measurement - Relative Humidity
- [ZBS-288] [ZCL8][4][0x0406] Occupancy Sensing
- [ZBS-289] [ZCL8][4][0x0b04] Electrical Measurement
- [ZBS-294] [ZCL8][5][0x0300] Color Control
- [ZBS-297] [ZCL8][6][0x0201] Thermostat
- [ZBS-298] [ZCL8][6][0x0202] Fan Control
- [ZBS-299] [ZCL8][6][0x0203] Dehumidification
- [ZBS-300] [ZCL8][6][0x0204] Thermostat UI Configuration
- [ZBS-301] [ZCL8][7][0x0100] Shade Configuration
- [ZBS-302] [ZCL8][7][0x0101] Door Lock
- [ZBS-303] [ZCL8][7][0x0102] Window Covering
- [ZBS-305] [ZCL8][8][0x0500] IAS Zone
- [ZBS-306] [ZCL8][8][0x0501] IAS ACE
- [ZBS-307] [ZCL8][8][0x0502] IAS WD
- [ZBS-314] [ZCL8][10][0x0700] SE Price
- [ZBS-315] [ZCL8][10][0x0701] SE DRLC
- [ZBS-316] [ZCL8][10][0x0702] SE Metering
- [ZBS-317] [ZCL8][10][0x0703] SE Messaging
- [ZBS-318] [ZCL8][10][0x0704] SE Tunneling
- [ZBS-319] [ZCL8][10][0x0800] SE Key Establishment
- [ZBS-320] [ZCL8][10][0x0705] SE Prepayment
- [ZBS-321] [ZCL8][10][0x0707] SE Calendar
- [ZBS-322] [ZCL8][10][0x0708] SE Device Management
- [ZBS-323] [ZCL8][10][0x0709] SE Events
- [ZBS-324] [ZCL8][10][0x070b] SE Sub-GHz
- [ZBS-326] [ZCL8][11][0x0019] OTA Upgrade
- [ZBS-348] [ZCL8][15][0x0b02] EN50523 Appliance Events and Alerts
- [ZBS-381] IAS Zone Cluster issues: add additional check - ensure command is sent from IAS CIE address
- [ZBS-382] IAS Zone Cluster issues: update the authorization check
- [ZBS-383] IAS Zone Cluster issues: deny all bind/unbind requests which relate to IAS Zone Cluster
- [ZBS-410] [ZCL8] Update according to Table 2-12. Enumerated Command Status Values
- [ZBS-537] Improve long attributes (>sizeof(zb_zcl_attr_val_t) bytes) reporting
- [ZBS-540] IAS Zone Cluster issues: Update related HA samples
- [ZBS-543] Remove APS groups API from scenes sample
- [ZBS-544] Remove APS binding API from light samples
- [ZBS-546] Replace APS binding API with ZDO binding API in the smart_plug sample
- [ZBS-547] ZDO groups API is not accessible from NCP Host
- [ZBS-732] Regression test for orphan scan (RTP_MAC_07)
- [ZBS-735] [ZCL_BC] Add REVERT_CLUSTER_ROLE to peer callback function
- [ZBS-753] [ZCL_BC] Fix tests with incompatible EXT attributes declarations
- [ZBS-782] NCP: implement a command for zb_set_max_joins
Sub-task:
- [ZBS-488] Fix validation script for ha_temperature_sensor sample
Question:
- [ZBS-541] [ZCL8] Identify mechanism for revision synchronization (ramp-up)
Bugfixes:
- [ZBS-222] Issues found inside scenes_zc.c
- [ZBS-409] [ZCL8] Missing processing of special case of MAINS_VOLTAGE_MIN_THRESHOLD in Power Configuration Cluster
- [ZBS-444] [ZCL][Scenes] SceneValid attribute is not updated
- [ZBS-502] Mgmt leave processing algorithm for ZRs and non-sleepy ZEDs
- [ZBS-631] Incorrect Read Attributes Response on reading multiple attributes when first is unsupported
- [ZBS-784] Fix packing ZB_ZDO_SIGNAL_DEVICE_ANNCE signal
- [ZBS-916] [API] Missing defgroup inclusion for some ZB_ZCL_KEEP_ALIVE macros
Stories:
- [ZBS-553] Remove masks check for reserved fields
- [ZBS-560] [ZCL_BC] Update cluster revision for current version
- [ZBS-561] [ZCL_BC] Add convenient API to get cluster revision of peer cluster.
- [ZBS-562] [ZCL_BC] API and Sample of Send Command approach
- [ZBS-565] [ZCL_BC] Provide ZCL8 sample with full API.
- [ZBS-566] [ZCL_BC] Test: Manual testing all samples - old ZCL, new ZCL8, run in mixed setup.
- [ZBS-567] [ZCL_BC] Update Documentation for new API, samples.
- [ZBS-568] [ZCL_BC] Check existing samples using new version ZCL against ZUTH
- [ZBS-570] [ZCL_BC] Fix samples with incompatible EXT attributes declarations
- [ZBS-697] [ZCL_BC] Command ZCL statuses parsing in samples
- [ZBS-702] Fix ToDo: Don't use a pointer to zgpd_id in zb_gp_data_cfm_t
- [ZBS-708] [ZCL_BC] Add Public API ZCL function to map old ZCL statuses to latest
- [ZBS-838] Add trace formats
ZBOSS 3.11.1.0 version dated 01/28/2022
This is a ZBOSS certification-ready release.
Bugfixes:
- [ZBS-689] Device stuck in undefined state after receive leave packet just after device announcement
ZBOSS 3.11.0.0 version dated 01/19/2022
This is a ZBOSS engineering release.
Tasks:
- [ZBS-665] Introduce Macsplit protocol version
Improvements:
- [ZBS-367] [BDB301] Add checks for bdbNodeIsOnANetwork and return appropriate errors
- [ZBS-368] [BDB301] Change bdbScanDuration
- [ZBS-370] [BDB301] Modify bdbCommissioningMode
Bugfixes:
- [ZBS-75] ZR crashes during aging out a child
- [ZBS-397] Router assers if the former child sends data request
- [ZBS-405] ZR aborts on the active scanning after leaving the network with rejoin flag set to ZB_FALSE
- [ZBS-417] Unable to perfom OTA upgrade to the current version of ZBOSS due to NVRAM incompatibilities.
- [ZBS-510] Wonders of MAC TX power provider
- [ZBS-511] Check min/max values for attributes in Thermostat cluster
- [ZBS-555] Add ZCL Occupancy Sensing cluster implementation
- [ZBS-630] Malformed entries in rejoin request table
- [ZBS-639] secur_material_specified is not set by NCP host application
- [ZBS-664] [API] Missing defgroup definition for zdo_distributed_security
- [ZBS-667] ZBOSS fails OTA Test Case OTA-TC-17C - Rate limiting
- [ZBS-668] [API] Typo in "ZCL Preasure Measurement cluster"
ZBOSS 3.10.0.0 version dated 11/25/2021
This is a ZBOSS certification-ready release. ATTENTION: Added section Deprecated in the API Reference. See Items, which are supposed to be removed in a while.
Tasks:
- [ZBS-408] Create demo sample for Public API: zb_disable_distributed
Improvements:
- [ZBS-197] [DOC] Add API reference for NCP headers
- [ZBS-216] Use zb_uint8_t instead of zb_uint_t for IPC signalling bit mask
- [ZBS-219] Close FIXME on unclear use of ZB_SRC_MATCH_TBL_DROP
- [ZBS-243] Add IdentifyTime parameter to zb_bdb_finding_binding_target()
- [ZBS-380] Indicate more NVRAM read/write errors
- [ZBS-385] Add ability to prevent NVRAM page erasing
- [ZBS-388] Add osif function to get file size
- [ZBS-389] Put macsplit trace API under ifdef ZB_TRACE_LEVEL
- [ZBS-390] Make ZB_MAC_PENDING_QUEUE_SIZE configurable
- [ZBS-393] Make crc function accept const pointer
- [ZBS-394] Trace addr unlock errors
- [ZBS-413] Replace ZB_IC_GET_TYPE_FROM_REC with ZB_IC_GET_TYPE_FROM_OPT and remove definition
New Features:
- [ZBS-223] Public API: get the type of a network, distributed or centralized security
- [ZBS-224] Public API: dynamic TX power management
- [ZBS-226] Public API: get a device type
- [ZBS-227] ZBOSS signal on Permit Joining Request
- [ZBS-228] Public API: zb_disable_distributed
- [ZBS-236] New API: stop network steering or formation before the process is finished
Bugfixes:
- [ZBS-157] Out buffers are not released after sending active endpoints requests to an unknown address
- [ZBS-184] Bugfix: Frame Counter field in APS auxiliary header does not change in all frame retry attempts
- [ZBS-214] Doxygen warning in the NCP API documentation
- [ZBS-215] Unexpected type of return value of the zb_ncp_custom_response
- [ZBS-225] Device type is not read from NVRAM for monolithic build
- [ZBS-231] Strange condition in APS secure code
- [ZBS-238] [BDB] PrimaryChannelSet has no priority over SecondaryChannelSet in distributed security network
- [ZBS-377] Don't remove unreachable child
- [ZBS-378] NCP - vendor specific response structure is not accessible from host
- [ZBS-379] Fix compilation for ZC (regression of wwah fixes)
- [ZBS-387] Fix trace message
- [ZBS-391] Send macsplit trace only after boot indication
- [ZBS-406] [NRF52] Update SPI signautre according to NCP changes
- [ZBS-411] zb_get_buf_delayed returns incorrect status during OOM state
- [ZBS-443] Unable to set TX power through production config v1
ZBOSS 3.9.0.0 version dated 10/08/2021
This is a ZBOSS certification-ready release.
Tasks:
- [ZBS-159] Device association fail if the Request Key packet is retransmitted - Design and implement APS commands dups detection
- [ZBS-178] [SECUR] Prevent attack to going ZR out of capacity due to many joins/rejoins implement fix
- [ZBS-196] Remove links to non-public/non-existent samples from SDK samples
- [ZBS-364] MAC split SoC build for nRF52840 platform
Improvements:
- [ZBS-6] [buildsystem] Unify Options used by SDK, by CI and by developers
- [ZBS-62] Add NCP protocol version checks
- [ZBS-213] Network simulator: get rid of double initialization in the multitest
- [ZBS-361] Make ZBNCP_BIG_BUF_SIZE be configurable
- [ZBS-362] Add Linky sample in ZBOSS SDK
- [ZBS-363] Introduce RET_OPERATION_INTERRUPTED
Bugfixes:
- [ZBS-156] The nvram_offset field for GPPB cache is not checked before reading
- [ZBS-195] Unsolicited NCP commands are not handled correctly
- [ZBS-230] zb_sleep_now() incorrectly calculates sleep time on nrf52-bm platform
- [ZBS-245] TP/PED-14: Parent Annce intervals are calculated not precisely
- [ZBS-355] Fix WWAH rejoin algorithm implementation, fix izs_device (WWAH bugfix)
- [ZBS-356] Add NVRAM write after TC Connectivity change (WWAH bugfix)
- [ZBS-357] Add Trust Center for Cluster check (WWAH bugfix)
- [ZBS-358] Add PANID conflict resolution to support WWAH test 11 into sp device code (WWAH bugfix)
- [ZBS-359] Fix issue with compile warning for zb_osif_log_file_rotate
ZBOSS 3.8.0.0 version dated 08/30/2021
This is a ZBOSS certification-ready release.
Tasks:
- [ZBS-142] Getting neighbors' LQI and RSSI (zb_zdo_get_diag_data()) - Implement logic (option 1)
- [ZBS-145] [SECUR] Prevent rx-on-when-idle change on rejoin
- [ZBS-149] [SECUR] Disallow TC rejoins when in Distributed - Do fix in rejoin
- [ZBS-152] [SECUR] ZBOSS secur stmt: TC rejoin policy in 3.0 mode - Do fixes for Joiner and TC
- [ZBS-158] Stabilization for 08/23 release
Improvements:
- [ZBS-115] Use different memory configs with regression tests
- [ZBS-167] Definition of 2 internal functions don't correspond its declaration
- [ZBS-170] [Tests] Add shebang to shell scripts
- [ZBS-174] Add missing ZB_OSIF_SERIAL_FLUSH() to console monitor
- [ZBS-175] Add support for pressure measurement cluster
- [ZBS-176] [MAC Split] Remove compilation of zb_ecc.c for MAC Split SoC builds
- [ZBS-177] Allow to use default base path
- [ZBS-189] [ZBOSS][Devtools] win_com_dump can't decode trace logs from a file for Nordic and Zephyr logs
- [ZBS-190] Add default file path log prefix
- [ZBS-198] Fix API change issues to make API changes seamless
New Features:
- [ZBS-117] Expanding the capabilities of trace functions
- [ZBS-168] Allow a user to send customer-specified NCP commands
- [ZBS-169] Getting active nodes API
- [ZBS-173] [ZBOSS] PHY testing mode
Bugfixes:
- [ZBS-84] Do not check for address conflict until NWK frame is unencrypted successfully
- [ZBS-98] Rejoin after Leave+Rejoin at ZR is broken in r23 - maybe, in r22 also
- [ZBS-130] ZR may send Link Status between Leave packets
- [ZBS-131] OTA Upgrade End callback to be called only on success upgrade
- [ZBS-162] ZED apps compilation fix
- [ZBS-163] APS max frag size fix
- [ZBS-171] Simple descriptor check procedure. Binding perfomance on cluster match is found
- [ZBS-172] OTA Upgrade Started callback is not called on delayed Image Block Response
- [ZBS-191] GP Sink (simple_combo) tries to respond to GPD with ZCL Default response if a command wasn't handled by application
- [ZBS-209] Incorrect parsing of LEAVE command in nwk_handle_zed_leave_confirm
ZBOSS 3.7.0.0 version dated 07/07/2021
This is a ZBOSS certification-ready release.
Improvements:
- [ZOI-909] Unify TRACE logic for logs and the MAC level packet dumps
- [ZOI-926] Stabilization for 07/05 release
New Features:
- [ZOI-817] Implement NCP commands and adapters for Inter-PAN communication
Questions:
- [ZOI-846] Different NWK keys are used in encryption Rejoin Request and Rejoin Response
Bugfixes:
- [ZOI-529] Unlocking Trust Center address which is not locked
- [ZOI-669] Missing Trust Center Rejoin
- [ZOI-861] Deadlock in NCP frame fragmentation logic
- [ZOI-893] GPPB test case is not included in the R22 generic certification firmware
- [ZOI-894] Green Power functionality is broken in ZBOSS >= 3.5.2.0
- [ZOI-934] TP/PRO/BV-13 fails on the Link status interval checks
ZBOSS 3.6.0.0 version dated 06/03/2021
This is a ZBOSS certification-ready release.
Tasks:
- [ZOI-485] Handle lack of TX buffers problem
- [ZOI-820] Read NCP firmware version on ncp host side
Improvements:
- [ZOI-729] Separated debug features enabling
- [ZOI-759] [SNCP] Added SubGHz functionality
- [ZOI-760] [SNCP][SE] Enable SubGHz cluster
- [ZOI-761] [SNCP] Add new return statuses for ncp_ll_quant
- [ZOI-762] [SNCP] Update calibration value format
- [ZOI-763] [SNCP] Implement commands for reading/writing reserved area
- [ZOI-764] [SNCP] Rearrange GET NWK KEYS response result to set current NWK key at the first place
- [ZOI-765] [SNCP] Add LQI and RSSI to Network discovery response
- [ZOI-768] [SNCP] Fix MISRA violations for SNCP build
- [ZOI-770] [SNCP] refactor manufacture tests to support 2.4GHz and SubGHz bands
- [ZOI-771] [SNCP] apply calibration value for HF OSC
- [ZOI-772] [SNCP] implement auto-polling for ED timeout response
- [ZOI-815] Stabilization for 05/31 release
New Features:
- [ZOI-584] SE in certified ZBOSS Platform by separating SE library
Epic:
- [ZOI-758] [SNCP] merge dsr/sncp_phase6 to current
Bugfixes:
- [ZOI-682] [SDK] ZED name in onoff_server is not the same as described in readme.txt
- [ZOI-766] [SNCP] Fix a key in response on Get APS key by IEEE
- [ZOI-767] [SNCP] Fix incorrect initial value for ZB current channel, when requested before setting a channel
- [ZOI-769] [SNCP] fix ring buffer macro ZB_RING_BUFFER_BATCH_PUT
- [ZOI-799] Inconsistency in the usage of the ZB_[H,LE]TO[LE,H][16,32]_ONPLACE macros
- [ZOI-836] NCP host asserts if the Reset Request is retransmitted
ZBOSS 3.5.2.0 version dated 05/06/2021
This is a ZBOSS certification-ready release.
Improvements:
- [ZOI-668] Applications readme improvements
- [ZOI-693] Stabilization for 04/09 release
Tasks:
- [ZOI-692] TP/R22/BV-17 remove test
Bugfixes:
- [ZOI-637] WWAH Door Lock. Test 11. ZCL command response not received
- [ZOI-698] Incorrect APS ACK handling if the ACK is received before the transmission is completed
- [ZOI-636] WWAH Door Lock. Test 4. No Read Attribute response
- [ZOI-623] WWAH Door Lock. Test 19: OTA attempt breaks the test?
- [ZOI-677] WWAH Door Lock. Test 20. No Check-in Request
- [ZOI-273] tp_bdb_fb_pre_tc_01b: Test implementation does not follow the specification
- [ZOI-706] ZB_RANDOM_JTR is broken
- [ZOI-704] TP/PED/14
- [ZOI-428] WWAH DoorLock. Test 23: Configure all features: 2 commands failed
- [ZOI-708] TP/R22/BV-15 timings
Questions:
- [ZOI-684] TP/R21/BV-02 TP/R21/BV-11 Processing of unencrypted NWK frames Clarification
- [ZOI-676] TP/APS/BV-14-I Group Management-Group Addition- Rx Clarification
- [ZOI-646] TP/PRO/BV-11 Source Route Repair clarification
- [ZOI-657] TP/NWK/BV-08-I Buffering for Sleeping Children Clarification
- [ZOI-699] tp_bdb_fb_pre_tc_01b_dutzed
- [ZOI-687] TP/PED-1 Clarification
- [ZOI-642] TP/PRO/BV-06 Many-to-one Routing test issues
ZBOSS 3.5.1.0 version dated 02/26/2021
This is a ZBOSS certification-ready release.
Improvements:
- [ZOI-164] MISRA Rule 1.3 - zdo/zdo_disc_srv.c
- [ZOI-216] [MISRA] Rule 2.1 - Unreachable code to be justified or refactored
- [ZOI-513] Define error handling for zb_nwk_change_my_child_addr_process in conflict address process
- [ZOI-521] Fix remaining MISRA violations for NCP in SNCP
- [ZOI-525] build: Improve ZBOSS version auto-detection based on git tags
- [ZOI-537] Fix remaining MISRA violations for 'common' in SNCP
- [ZOI-538] Fix remaining MISRA violations for ZDO in SNCP
- [ZOI-558] Remove all references of ZB_B2U(ZB_FALSE) and ZB_B2U(ZB_TRUE)
- [ZOI-572] MISRA: Do not include code snippets source code tags for deviation records
- [ZOI-632] Stabilization for 03/12 release
Questions:
- [ZOI-280] zb_bufpool_mult_storage.c - rule 18.2 violation
- [ZOI-282] zbs_bl_image.c - rule 18.2 violation
Bugfixes:
- [ZOI-312] Partial data copy in zb_aps_hdr_mod
- [ZOI-314] Bind operations do not take addr redirect into account
- [ZOI-315] User's ZDO command complete callback can block NWK Input queue
- [ZOI-350] [MISRA] Rule 1.3 - zb_**bit_math.c
- [ZOI-378] tp_pro_bv-06 - Missing checks in test script
- [ZOI-542] doxygen: cond ZBOSS_INTERNAL without endcond in zboss_api.h
- [ZOI-596] ZBOSS stack fails Certification TP/R21/BV-13
- [ZOI-608] Suspicious placement inside application structure & commissioning start API section
- [ZOI-617] Clearing brrt structure brings memory corruption
- [ZOI-627] ZBOSS test scripts are not checking which APS link key was used to trasport the NWK key
ZBOSS 01/31/2021
This is a ZBOSS certification-ready release.
Improvements:
- [ZOI-185] Don't use named enums for constants
- [ZOI-238] Fix MISRA violations, Rule 13.5
- [ZOI-247] Prettify boolean-like macros with actual integer type
- [ZOI-293] Fix MISRA violations, Rule 14.3
- [ZOI-308] Fix MISRA violations, Rule 11.3
- [ZOI-338] Enhance Public NVRAM API
- [ZOI-340] Refactor ZB_NWK_SHORT_HDR_SIZE() for build without NWK multicast
- [ZOI-352] Fix MISRA violations, Rule 17.7
- [ZOI-373] Fix "fall through" switch clause in nwk_cr_permit_join.c, MISRA Rule 16.3
- [ZOI-384] Fix MISRA violations, Dir 4.3
- [ZOI-385] Fix MISRA violations, Rule 5.3
- [ZOI-386] Fix remaining MISRA Rule 8.2 violations in platform
- [ZOI-387] Fix MISRA violations, Rule 8.5
- [ZOI-389] Fix C-STAT MISRAC2012-Rule-9.1_f warnings
- [ZOI-397] Fix MISRA violations, Rule 11.9
- [ZOI-398] Fix MISRA violations, Rule 12.2
- [ZOI-399] Fix Rule 14.2 in zb_nvram.c (zb_get_nvram_page_count())
- [ZOI-400] MISRA Rule 14.4, fix bit checking in conditions
- [ZOI-401] Fix remaining violations for Rule 16.x
- [ZOI-403] Fix MISRA violations, Rule 18.1
- [ZOI-414] Fix MISRA violation Rule 17.7, function aps_*
- [ZOI-415] Fix MISRA violation Rule 17.7, function mac_*
- [ZOI-416] Fix MISRA violation Rule 17.7, for function zb_schedule_alarm_cancel
- [ZOI-430] Fix MISRA violation Rule 17.7, function ncp_*
- [ZOI-432] Fix MISRA violation Rule 17.7, function NOROM_*
- [ZOI-433] Fix MISRA violation Rule 17.7, function Power_*
- [ZOI-434] Fix MISRA violation Rule 17.7, function RF_*
- [ZOI-435] Fix MISRA violation Rule 17.7, function stop_single_command
- [ZOI-471] Fix MISRA violation Rule 17.7, function zb_address_lock and zb_address_unlock
- [ZOI-480] Fix MISRA violation Rule 17.7, function zb_address_by_ieee, zb_address_by_short and zb_address_ieee_by_short
- [ZOI-502] zb_ecc: MISRA Rule 14.3 violation for async mode
- [ZOI-503] MISRA: Add Rule 14.3 deviation records for platform-dependent code
- [ZOI-517] Fix MISRA violation Rule 17.7, function zb_nvram_*
- [ZOI-518] Fix MISRA violation Rule 17.7, function zb_nwk_*
- [ZOI-518] Fix MISRA violation Rule 17.7, function zb_nwk_*
- [ZOI-574] Stabilization for 02/08 release
New Features:
- [ZOI-369] Implement error propagation system
- [ZOI-494] Fix MISRA violation Rule 17.7, function zb_address_update, zb_address_delete and zb_address_set_pan_id
- [ZOI-495] Fix MISRA violation Rule 17.7, function zb_buf_alloc_*, zb_buf_cut_left_func and zb_buf_reuse_func
- [ZOI-498] Fix MISRA violation Rule 17.7, function zb_channel_*
- [ZOI-506] Fix MISRA violation Rule 17.7, function zb_kec_*
- [ZOI-522] ZBOSS secur stmt - TC authenticates Joiner only is network is open
Tasks:
- [ZOI-197] ZBOSS API CHANGE: Descriptor management commands and adapters
- [ZOI-208] Host-side Prod config logic
- [ZOI-209] Prepare and debug NCP SDK samples
- [ZOI-222] PAN ID Conflict resolution commands and adapters
- [ZOI-223] MTORR commands and adapters
- [ZOI-224] zb_nwk_get_parent() adapter
- [ZOI-306] Diagnostics values support
- [ZOI-331] Debug some HA Samples for NCP architecture
- [ZOI-349] Use the same ZBOSS Core library for monolithic and NCP SoC builds
- [ZOI-383] [MISRA] Rule 13.5 - Wrong error supression
- [ZOI-441] [MISRA] Rule 1.3 - aps_main.c - Division by zero
- [ZOI-478] Add C-STAT configuration to the report
- [ZOI-482] Enable on-SoC GPPB with testing against GPTH
- [ZOI-212] Checking behaviour of the Light Sample for NCP architecture
- [ZOI-214] Checking behaviour of the On/Off sample for NCP architecture
- [ZOI-332] Debug test_sample_1
Bugfixes:
- [ZOI-81] ZBOSS secur stmt: panid conflict resolution and NWK manager policy
- [ZOI-82] ZBOSS secur stmt: sample apps for panid conflict resolution settings
- [ZOI-295] NCP host should handle communication port reattachment during NCP reset
- [ZOI-473] ZR kicks out child ZED if it doesn't set keep-alive timeout option
- [ZOI-475] Light Sample and On/Off Server SDK samples debugging for NCP
- [ZOI-497] Get rid of ZB_PRO_TESTING_MODE define
- [ZOI-515] Deadlocks in ZB_INTERRUPT_SAFE_BUFS and ZB_INTERRUPT_SAFE_ALARMS
- [ZOI-535] Mesh routing is not initialized properly for NCP SoC with a ZC role
- [ZOI-543] Sample build with common libzboss don't exchange TC Link Key
- [ZOI-557] Failing tp_154_mac_data_02
- [ZOI-559] [GP][Sink][ZUTH] Sink stops functioning after reception Application Description
- [ZOI-560] Malformed Route Records in case of enabled MTORR and inability to find the last element in Route Discovery Table
- [ZOI-586] APS User Payload feature is broken
ZBOSS 12/30/2020
This is a ZBOSS certification-ready release.
Improvements:
- [ZOI-186] Make ZCL functionality optional for NCP
- [ZOI-220] [MISRA] Rule 8.2 - zdo_common.c
- [ZOI-483] Stabilization for December's release
- [ZOI-486] Change a ZBOSS SDK versioning model
New Features:
- [ZOI-470] [SNCP] Indication of remote ZDO requests
Tasks:
- [ZOI-203] Implement Device Authorized and Device Update signals for NCP host
- [ZOI-204] Implement ZDO_SIGNAL_LEAVE signal for NCP host
- [ZOI-221] ZBOSS API CHANGE: Security-related adapters and commands
- [ZOI-287] Debug Regression tests for NCP architecture
Questions:
- [ZOI-59] The usage of max_size argument inside scheduler API
Bugfixes:
- [ZOI-140] [DOC] Install code functions are missing in API reference since SDK v4.0
- [ZOI-215] Access a buffer after freeing during indirect transmission
- [ZOI-270] tp_bdb_cn_nsa_tc-01d_dutzr: Fails if the THr1 associates via DUT
- [ZOI-334] R22 cert - r21_bv_11_dut_zc weird node desc req
- [ZOI-379] TP/SEC/BV-26-I: Fix test procedure
- [ZOI-380] Device asserts in case of absent APS ack during fragmented transmission
- [ZOI-395] Buf leak in the ZDO channel manager.
- [ZOI-427] Wrong check for valid ranges in osif_nvram_xxx
- [ZOI-458] Fix app description table erasing
- [ZOI-469] [SNCP] Fragmented APS TX stabilization
- [ZOI-487] Simple combo doesn't work with -O3 options
- [ZOI-488] Moving diagnostics structures
ZBOSS 11/30/2020
This is a ZBOSS certification-ready release.
Improvements:
- [ZOI-285] Disable C-STAT diagnostics from TI SDK
- [ZOI-260] Fix MISRA violations, Rule 16.3
- [ZOI-235] Fix MISRA violations, Rule 16.4
- [ZOI-279] Fix MISRA violations, rules 5.5, 5.6, 5.7, 5.8
- [ZOI-243] Refactor zb_schedule_callback() interface
- [ZOI-290] Improve deviation record format
- [ZOI-367] Stabilization for November's release
Tasks:
- [ZOI-226] Implement zb_bdb_reset_via_local_action() for NCP Host
- [ZOI-195] Implement TC Policy commands and adapters
- [ZOI-206] Implement on-SoC NVRAM access
- [ZOI-225] Missing ZDO adapters and commands
- [ZOI-199] Set max children command: transport and adapters (incorporate into startup sequence)
Sub-tasks:
- [ZOI-286] Debug some HA samples for NCP architecture
- [ZOI-213] Checking behaviour of the Simple GW application for NCP architecture
Bugfixes:
- [ZOI-255] Compilation error for ncp_hl_proto.c (incompatible __packed arg)
- [ZOI-358] win_com_dump does not work with firmware build using GCCv9+
- [ZOI-246] ncp_hl_proto.c: Use of uninitialized 'buf' variable
- [ZOI-276] TH Extend set duration in tp_ped-14_dutzc, dutzr tests
- [ZOI-245] ncp_hl_proto.c: Use of uninitialized 'rh' variable
- [ZOI-301] Fix Macro redefinition warning during cstat build
- [ZOI-364] tp_bdb_fb_pre_tc_02: Fails due to the lack of time between Device Announcement and Leave command
- [ZOI-322] Incorrect return value in zdo_mgmt_leave_cli() if 'cb' == NULL
- [ZOI-297] ZBOSS assert after receiving the leave command
- [ZOI-188] LIGHT_CONTROL_START_SEARCH_LIGHT disabled by default in the Light_sample/Light_controller
ZBOSS 11/03/2020
This is a ZBOSS certification-ready release.
Improvements:
- [ZOI-155] Put zb_debug_bcast_key() under DEBUG define
- [ZOI-157] Fix ZBOSS stack MISRA violations for Rule 2.2
- [ZOI-158] Fix ZBOSS stack MISRA violations for Rule 14.2
- [ZOI-160] Fix MISRA ZBOSS violations for Rule 8.3
- [ZOI-161] Merge fixes for violations of mandatory rules
- [ZOI-165] Fix MISRA violations, rule 14.4
- [ZOI-166] Fix MISRA violations, Rule 15.6
- [ZOI-169] Fix MISRA ZBOSS violations for Rule 8.4
- [ZOI-176] Use _Bool C type for zb_bool_t instead of enum for C99
- [ZOI-177] Remove ZB_LITE_NO_JOIN_ZR_AS_ZED and related code
- [ZOI-184] Fix MISRA violations for rule 2.1
- [ZOI-187] Design definition of deviation records for MISRA
- [ZOI-218] Fix MISRA violations for Rule 8.2
- [ZOI-219] Fix MISRA violations for Directive 4.10
- [ZOI-227] Fix MISRA violations, Rule 3.1
- [ZOI-236] Fix MISRA violations, Rule 9.2
- [ZOI-237] Fix MISRA violations, Rule 9.3
- [ZOI-250] r22_cert_tests_gcc_build: Compilation error due to failure finding nwk_internal.h
- [ZOI-261] Including OSIF sources to NCP SDK
Tasks:
- [ZOI-156] Change DSR copyright in ZBOSS sources
- [ZOI-175] Provide release notes within zboss_doc
- [ZOI-181] Add .clang-format configuration for coding style
- [ZOI-192] Enable ZCL reporting in NCP
- [ZOI-193] ZBOSS API CHANGE: Refactor bind table inquirement logic (zb_zdo_find_bind_src(), zb_check_binding(), etc)
- [ZOI-194] Implement Poll Interval Management Adapters
- [ZOI-196] APS Group Management adapters
- [ZOI-198] Leave related commands: transport and adapters
Sub-tasks:
- [ZOI-210] Checking behaviour of the Scenes application for NCP architecture
- [ZOI-211] Checking behaviour of the Thermostat application for NCP architecture
Bugfixes:
- [ZOI-141] [DOC] Bug in "Zigbee API for code security installation" section
- [ZOI-172] APS update device memory leak
- [ZOI-217] Link Status is not sent when device type is unknown
- [ZOI-254] GP Sink: Erroneous waiting for a Application Description frame
ZBOSS 10/06/2020
This is a ZBOSS certification-ready release.
Improvements:
- [ZOI-180] Stabilization for September's release
New features:
- [ZOI-84] ZBOSS secur stmt: "ED timeout request" keepalive
- [ZOI-144] Build Zigbee PRO R22 test firmware for NCS platform
- [ZOI-148] [ZBOSS] Green Power Combo as a separate library
Tasks:
- [ZOI-99] Rework conditionals in dev guide and API docs
- [ZOI-139] [ZBOSS] Separation GPPB and GPCB libraries
Bugfixes:
- [ZOI-80] The value returned by zb_bdb_is_factory_new() is not updated
- [ZOI-93] ED Timeout keepalive method disables polling for rx_off end device
- [ZOI-94] No packet sending between two local EPs in one group
- [ZOI-102] The ZB_ZCL_DECLARE_POWER_CONFIG_ATTRIB_LIST() causes compilation errors
- [ZOI-137] Device gets kicked out of the network if it does not finish the first association
- [ZOI-145] Memory corruption in ZCL callback
- [ZOI-147] ZB_ZDO_SIGNAL_DEVICE_AUTHORIZED is not generated for legacy devices
- [ZOI-168] ZBOSS generates malformed packets if it receives a Route Request with an extended destination address
- [ZOI-170] Fix unknown device type for neighbour
- [ZOI-171] End device generates invalid network address request if application tries to communicate with an unreachable device
ZBOSS 09/10/2020
This is a ZBOSS certification-ready release.
New features:
- [ZOI-138] [ZBOSS] Green Power Update (v1.1)
Tasks:
- [ZOI-71] [API docs] Add details documentation for ZGP API
- [ZOI-115] [SNCP] Update monolythic C tests for standalone NCP
- [ZOI-116] [SNCP] Port RPi SPI transport from svn to ZOI codebase
- [ZOI-117] [SNCP] Port Manufacturer mode from svn codebase
- [ZOI-118] [SNCP] Improve NCP LL library API documentation
- [ZOI-119] [SNCP] Optimize SNCP flash usage by cutting features
- [ZOI-120] [SNCP] Rework python tests set
- [ZOI-121] [SNCP] Change commands blocking logic
- [ZOI-122] [SNCP] "expose all keys" debug feature
- [ZOI-134] [SNCP] Save device role and rx-on-when-idle in NVRAM in NCP mode
- [ZOI-136] [SNCP] Add into ZOI codebase OTA file generation tool from svn
Bugfixes:
- [ZOI-95] An issue with reporting between two local EPs
- [ZOI-104] Bug in zb_bdb_reset_via_local_action() function
- [ZOI-111] Using more than 10 entries of reporting configuration leads to NVRAM corruption
- [ZOI-113] Corrupted firmware pointer in OTA handler
- [ZOI-123] ZC can change its address during conflict resolution
- [ZOI-124] [SNCP] Compiler warnings fix
- [ZOI-125] Wrong implementetion of endian conversion in NWK for BE machine
- [ZOI-126] [SNCP] Sync rx on/off with MAC after setting via NCP
- [ZOI-127] More ZED role runtime checks
- [ZOI-128] [SNCP] Indicate address update after address conflict in ZED role
- [ZOI-129] [SNCP] Sniffer mode does not work
- [ZOI-130] No APSDE-DATA.conf after sending APS packet to myself via binding
- [ZOI-131] [SNCP] Unnecessary alarms waking NCP in ZED mode
- [ZOI-132] [SNCP] Reduce buffers used by NCP LL
- [ZOI-133] Non-sleepy ZED drops Device Annce
- [ZOI-135] [SNCP] Update ZDO descriptors after changing rx-on
ZBOSS 08/03/2020
This is a ZBOSS monthly release.
Improvements:
- [ZOI-51] New look to Makefiles in mk/xxx dirs
- [ZOI-79] Get rid of ZB_SCHEDULE_APP_ALARM_CANCEL_AND_GET_BUF.
New features:
- [ZOI-105] NCP Host: Exclude NVRAM from PoC
- [ZOI-106] NCP Host: Create NCP Host build
- [ZOI-107] NCP Host: Implement BDB commissioning
- [ZOI-108] NCP Host: Implement commands serialization (partially)
- [ZOI-109] NCP Host: Compile On/Off sample
- [ZOI-110] NCP Host: Run On/Off sample
Tasks:
- [ZOI-62] [API docs] Improve the documentation of ZB_ZCL_ATTR_ACCESS_WRITE_OPTIONAL flag
- [ZOI-64] [API docs] Add table for clusters/callbacks
Bugfixes:
- [ZOI-46] Frame counters are not reset after NWK key exchange
- [ZOI-63] Address unlock issue for ZDO MGMT Leave req
- [ZOI-72] [API docs] TRACE_DATA_FORMAT_ADDITIONAL is not added to group
- [ZOI-75] Fix if and cond number mismatch in API headers
- [ZOI-101] The ZDO_MATCH_DESC_REQ NCP command's response does not contain responder's short address
ZBOSS 07/14/2020
This is the first ZBOSS certification-ready release.
Improvements:
- [ZOI-31] Extend serial with asynchronous/buffered API
- [ZOI-32] Reduce the number of NCP transport interfaces
New features:
- [ZOI-34] Add serial transport for NCP - SoC side
Tasks:
- [ZOI-69] Binding to the wrong cluster is possible.
Bugfixes:
- [ZOI-13] The usage of channel_mask inside production config
- [ZOI-14] HTTPS not available at zoi home page
- [ZOI-16] Periodic reporting attributes does not work if binding performed after reporting max interval
- [ZOI-19] Unable to define ZB_MAC_GET/SET_RSSI from platform_mac.h file
- [ZOI-20] Compile time issue once ZB_MAC_RX_QUEUE_CAP is disabled
- [ZOI-28] Suspicious authorization signals
- [ZOI-35] Can't configure reporting on multi-endpoint device
- [ZOI-36] Unable to compile ZR-only role if APS fragmentation is enabled
- [ZOI-38] Unable to compile ZC_only role due to linker issues
- [ZOI-42] internals_doc visible for some API elements
- [ZOI-43] API docs: Typos in documentation
- [ZOI-44] ZCL Occupancy Sensing cluster implementation seems to be missing
- [ZOI-60] Network permits new devices after device leave
- [ZOI-73] It is impossible to initialize both Control4 cluster and Power Config Cluster
- [ZOI-76] Fix zb_config.h API doc issues
- [ZOI-78] BDB status not cleaned by Leave or Factory Reset after F&B target start
ZBOSS 07/07/2020
This is a ZBOSS monthly release. Release notes were not generated for this version.
ZBOSS 06/30/2020
This is a ZBOSS monthly release. Also, it is the first release that was based on the stabilized ZBOSS version.