GPD Commissioning params for Application approval. More...
#include <zboss_api_zgp.h>
GPD Commissioning params for Application approval.
| zb_uint8_t zgp_approve_comm_params_s::actions |
Pairing configuration actions
| zb_zgp_cluster_list_t zgp_approve_comm_params_s::cluster_list |
ZGPD Cluster list
| zb_uint8_t zgp_approve_comm_params_s::device_id |
ZGPD device ID
| zb_zgp_gpd_cmds_list_t zgp_approve_comm_params_s::gpd_cmds_list |
ZGPD Command list
| zb_ieee_addr_t zgp_approve_comm_params_s::ieee_addr |
ZGPD long IEEE address if available, otherwise filled with zeroes
| zb_uint16_t zgp_approve_comm_params_s::manuf_id |
Manufacturer ID (meaningful if device_id = 0xFE or 0xFF)
| zb_uint16_t zgp_approve_comm_params_s::manuf_model_id |
Manufacturer model ID (meaningful if device_id = 0xFE or 0xFF)
| zb_uint8_t zgp_approve_comm_params_s::num_of_endpoints |
Pairing configuration number of paired endpoints field
| zb_uint8_t zgp_approve_comm_params_s::num_of_reports |
total number of different report descriptors that GPD sent during the commissioning process
| zb_bool_t zgp_approve_comm_params_s::pairing_configuration |
It is ZB_TRUE in case this approve signal was triggered by GP Pairing Configuration command
| zb_uint8_t zgp_approve_comm_params_s::pairing_endpoint |
Device endpoint, on which commissioning is currently active
| zgp_raw_report_desc_t zgp_approve_comm_params_s::reports[ZB_ZGP_APP_DESCR_REPORTS_NUM] |
array of reports
| zb_zgpd_id_t zgp_approve_comm_params_s::zgpd_id |
ZGPD ID