Logo
Developing with ZBOSS for Zigbee
zb_zll_commissioning_reset_to_fn_s Struct Reference

Parsed Commissioning.ResetToFactoryNewRequest payload. More...

#include <zb_zcl_touchlink_commissioning.h>

Data Fields

zb_uint32_t trans_id
 Inter-PAN transaction identifier.
 

Detailed Description

Parsed Commissioning.ResetToFactoryNewRequest payload.

See also
ZCL spec, subclause 13.3.2.1.4.

The documentation for this struct was generated from the following file: