Parsed Commissioning.NetworkJoinEndDeviceRequest payload. More...
#include <zb_zcl_touchlink_commissioning.h>
Parsed Commissioning.NetworkJoinEndDeviceRequest payload.
| zb_uint8_t zb_zll_commissioning_network_join_end_device_req_s::channel |
Logical channel.
| zb_uint8_t zb_zll_commissioning_network_join_end_device_req_s::encr_nwk_key[16] |
Encrypted network key.
| zb_ext_pan_id_t zb_zll_commissioning_network_join_end_device_req_s::ext_pan_id |
Extended Pan ID.
| zb_uint16_t zb_zll_commissioning_network_join_end_device_req_s::free_group_ids_begin |
Free group identifiers range begin.
| zb_uint16_t zb_zll_commissioning_network_join_end_device_req_s::free_group_ids_end |
Free group identifiers range end.
| zb_uint16_t zb_zll_commissioning_network_join_end_device_req_s::free_nwk_addrs_begin |
Free network address range begin.
| zb_uint16_t zb_zll_commissioning_network_join_end_device_req_s::free_nwk_addrs_end |
Free network address range end.
| zb_uint16_t zb_zll_commissioning_network_join_end_device_req_s::group_ids_begin |
Group identifiers begin.
| zb_uint16_t zb_zll_commissioning_network_join_end_device_req_s::group_ids_end |
Group identifiers end.
| zb_uint8_t zb_zll_commissioning_network_join_end_device_req_s::key_idx |
Key index.
| zb_uint8_t zb_zll_commissioning_network_join_end_device_req_s::nwk_upd_id |
Network update identifier.
| zb_uint16_t zb_zll_commissioning_network_join_end_device_req_s::pan_id |
Pan ID.
| zb_uint16_t zb_zll_commissioning_network_join_end_device_req_s::short_addr |
Network address.
| zb_uint32_t zb_zll_commissioning_network_join_end_device_req_s::trans_id |
Inter-PAN transaction identifier.