Logo
Developing with ZBOSS for Zigbee
zb_zll_commissioning_get_endpoint_list_req_s Struct Reference

Parsed Commissioning.GetEndpointListRequest payload. More...

#include <zb_zcl_touchlink_commissioning.h>

Data Fields

zb_uint8_t start_idx
 

Detailed Description

Parsed Commissioning.GetEndpointListRequest payload.

See also
ZCL spec, subclause 13.3.2.1.10.

Field Documentation

§ start_idx

zb_uint8_t zb_zll_commissioning_get_endpoint_list_req_s::start_idx

Start index.


The documentation for this struct was generated from the following file: