Logo
Developing with ZBOSS for Zigbee
zb_zll_commissioning_endpoint_info_record_s Struct Reference

Endpoint information record for Commissioning.GetEndpointListResponse command. More...

#include <zb_zcl_touchlink_commissioning.h>

Data Fields

zb_uint16_t addr_short
 
zb_uint8_t endpoint
 
zb_uint16_t profile_id
 
zb_uint16_t device_id
 
zb_uint8_t version
 

Detailed Description

Endpoint information record for Commissioning.GetEndpointListResponse command.

See also
ZCL spec, subclause 13.3.2.2.8.

Field Documentation

§ addr_short

zb_uint16_t zb_zll_commissioning_endpoint_info_record_s::addr_short

Network address.

§ device_id

zb_uint16_t zb_zll_commissioning_endpoint_info_record_s::device_id

Device identifier.

§ endpoint

zb_uint8_t zb_zll_commissioning_endpoint_info_record_s::endpoint

Endpoint identifier.

§ profile_id

zb_uint16_t zb_zll_commissioning_endpoint_info_record_s::profile_id

Profile identifier.

§ version

zb_uint8_t zb_zll_commissioning_endpoint_info_record_s::version

Version.


The documentation for this struct was generated from the following file: