Logo
Developing with ZBOSS for Zigbee
zb_zll_commissioning_device_information_ep_info_res_s Struct Reference

Parsed device information record from the Commissioning.DeviceInformationResponse payload. More...

#include <zb_zcl_touchlink_commissioning.h>

Data Fields

zb_ieee_addr_t ieee_addr
 
zb_uint8_t ep_id
 
zb_uint16_t profile_id
 
zb_uint16_t device_id
 
zb_uint8_t version
 
zb_uint8_t group_id_count
 
zb_uint8_t sort
 

Detailed Description

Parsed device information record from the Commissioning.DeviceInformationResponse payload.

See also
ZCL spec, subclause 13.3.2.2.2.

Field Documentation

§ device_id

zb_uint16_t zb_zll_commissioning_device_information_ep_info_res_s::device_id

Device identifier.

§ ep_id

zb_uint8_t zb_zll_commissioning_device_information_ep_info_res_s::ep_id

Device's endpoint identifier.

§ group_id_count

zb_uint8_t zb_zll_commissioning_device_information_ep_info_res_s::group_id_count

Group identifier count.

§ ieee_addr

zb_ieee_addr_t zb_zll_commissioning_device_information_ep_info_res_s::ieee_addr

IEEE address of the sub-device.

§ profile_id

zb_uint16_t zb_zll_commissioning_device_information_ep_info_res_s::profile_id

Profile identifier.

§ sort

zb_uint8_t zb_zll_commissioning_device_information_ep_info_res_s::sort

Sort.

§ version

zb_uint8_t zb_zll_commissioning_device_information_ep_info_res_s::version

Device version.


The documentation for this struct was generated from the following file: