Logo
Developing with ZBOSS for Zigbee
zb_zll_commissioning_device_information_common_res_s Struct Reference

Parsed permanent part of the Commissioning.DeviceInformationResponse payload. More...

#include <zb_zcl_touchlink_commissioning.h>

Data Fields

zb_uint32_t trans_id
 Inter-PAN transaction identifier.
 
zb_uint8_t n_subdevs
 Number of sub-devices.
 
zb_uint8_t start_idx
 Start index.
 
zb_uint8_t n_records
 Device information record count.
 

Detailed Description

Parsed permanent part of the Commissioning.DeviceInformationResponse payload.

See also
ZCL spec, subclause 13.3.2.2.2.

The documentation for this struct was generated from the following file: