Logo
Developing with ZBOSS for Zigbee
zb_zgps_mapping_entry_additional_info_s Struct Reference

Mapping table entry additional info structure Figure 82 – Format of the Additional information block field of the Translation Table entry. More...

#include <zboss_api_zgp.h>

Data Fields

zb_uint8_t length
 

Detailed Description

Mapping table entry additional info structure Figure 82 – Format of the Additional information block field of the Translation Table entry.


The documentation for this struct was generated from the following file: