Logo
Developing with ZBOSS for Zigbee
zb_zgps_mapping_entry_additional_info_option_selector_s Struct Reference

Mapping table entry additional info option selector structure Figure 84 – Format of the Option selector field of the Option record field of the Translation Table entry. More...

#include <zboss_api_zgp.h>

Data Fields

zb_bitfield_t option_length:4
 
zb_bitfield_t option_id:4
 

Detailed Description

Mapping table entry additional info option selector structure Figure 84 – Format of the Option selector field of the Option record field of the Translation Table entry.


The documentation for this struct was generated from the following file: