Logo
Developing with ZBOSS for Zigbee
zb_zgp_cluster_list_s Struct Reference

GPD Cluster List. More...

#include <zboss_api_zgp.h>

Data Fields

zb_uint8_t server_cl_num
 
zb_uint8_t client_cl_num
 
zb_uint16_t server_clusters [ZB_ZGP_MAX_PAIRED_CONF_CLUSTERS]
 
zb_uint16_t client_clusters [ZB_ZGP_MAX_PAIRED_CONF_CLUSTERS]
 

Detailed Description

GPD Cluster List.

Field Documentation

§ client_cl_num

zb_uint8_t zb_zgp_cluster_list_s::client_cl_num

Number of client ClusterIDs

§ client_clusters

zb_uint16_t zb_zgp_cluster_list_s::client_clusters[ZB_ZGP_MAX_PAIRED_CONF_CLUSTERS]

ClusterID List Client

§ server_cl_num

zb_uint8_t zb_zgp_cluster_list_s::server_cl_num

Number of server ClusterIDs

§ server_clusters

zb_uint16_t zb_zgp_cluster_list_s::server_clusters[ZB_ZGP_MAX_PAIRED_CONF_CLUSTERS]

ClusterID List Server


The documentation for this struct was generated from the following file: