Leave Indication parameters. More...
#include <zboss_api_zdo.h>
Data Fields | |
| zb_uint16_t | short_addr |
| zb_ieee_addr_t | device_addr |
| zb_uint8_t | rejoin |
Leave Indication parameters.
Stack passes this parameter to application upon receipt of leave indication primitive.
| zb_ieee_addr_t zb_zdo_signal_leave_indication_params_s::device_addr |
Long address of device requested to leave or leaving device
| zb_uint8_t zb_zdo_signal_leave_indication_params_s::rejoin |
1 if this was leave with rejoin; 0 - otherwise
| zb_uint16_t zb_zdo_signal_leave_indication_params_s::short_addr |
Short address of device requested to leave or leaving device