Logo
Developing with ZBOSS for Zigbee

Association parameters. More...

#include <zboss_api_zdo.h>

Data Fields

zb_uint16_t device_short_addr
 
zb_ieee_addr_t ieee_addr
 
zb_uint8_t capability
 

Detailed Description

Association parameters.

Stack passes this parameter to application when some device joins/rejoins to network.

Field Documentation

§ device_short_addr

zb_uint16_t zb_zdo_signal_device_annce_params_s::device_short_addr

address of device that recently joined to network


The documentation for this struct was generated from the following file: