Logo
Developing with ZBOSS for Zigbee

Sleep signal parameters. More...

#include <zboss_api_zdo.h>

Data Fields

zb_uint32_t sleep_tmo
 

Detailed Description

Sleep signal parameters.

Stack passes this parameter to application when device ready to sleep.

Field Documentation

§ sleep_tmo

zb_uint32_t zb_zdo_signal_can_sleep_params_s::sleep_tmo

sleep duration in milliseconds


The documentation for this struct was generated from the following file: