Logo
Developing with ZBOSS for Zigbee
zb_zdo_raw_req_param_s Struct Reference

Parameters for zb_zdo_raw_req call. More...

#include <zboss_api_zdo.h>

Data Fields

zb_uint16_t cluster_id
 
zb_uint16_t dst_addr
 

Detailed Description

Parameters for zb_zdo_raw_req call.

Field Documentation

§ cluster_id

zb_uint16_t zb_zdo_raw_req_param_s::cluster_id

The identifier of the object for which this frame is intended.

§ dst_addr

zb_uint16_t zb_zdo_raw_req_param_s::dst_addr

Destination address


The documentation for this struct was generated from the following file: