Parameters of Power_desc_req primitive. More...
#include <zboss_api_zdo.h>
Data Fields | |
| zb_uint16_t | nwk_addr |
Parameters of Power_desc_req primitive.
To be put into buffer as data (means - after space alloc).
| zb_uint16_t zb_zdo_power_desc_req_s::nwk_addr |
NWK address that is used for IEEE address mapping.