Parameters for Mgmt_NWK_Update_req. More...
#include <zboss_api_zdo.h>
Data Fields | |
| zb_zdo_mgmt_nwk_update_req_hdr_t | hdr |
| zb_uint8_t | scan_count |
| zb_uint16_t | manager_addr |
| zb_uint16_t | dst_addr |
Parameters for Mgmt_NWK_Update_req.
| zb_uint16_t zb_zdo_mgmt_nwk_update_req_s::dst_addr |
Destination address
| zb_zdo_mgmt_nwk_update_req_hdr_t zb_zdo_mgmt_nwk_update_req_s::hdr |
Request header
| zb_uint16_t zb_zdo_mgmt_nwk_update_req_s::manager_addr |
This field shall be present only if the ScanDuration is set to 0xff, and, where present, indicates the NWK address for the device with the Network Manager bit set in its Node Descriptor.
| zb_uint8_t zb_zdo_mgmt_nwk_update_req_s::scan_count |
This field represents the number of energy scans to be conducted and reported