Match_desc_req head. More...
#include <zboss_api_zdo.h>
Data Fields | |
| zb_uint16_t | nwk_addr |
| zb_uint16_t | profile_id |
| zb_uint8_t | num_in_clusters |
Match_desc_req head.
| zb_uint8_t zb_zdo_match_desc_req_head_s::num_in_clusters |
The number of Input Clusters provided for matching within the InClusterList.
| zb_uint16_t zb_zdo_match_desc_req_head_s::nwk_addr |
NWK address that is used for IEEE address mapping.
| zb_uint16_t zb_zdo_match_desc_req_head_s::profile_id |
Profile ID to be matched at the destination.