Parameters for ieee_addr_req command. More...
#include <zboss_api_zdo.h>
Data Fields | |
| zb_uint16_t | dst_addr |
| zb_uint16_t | nwk_addr |
| zb_uint8_t | request_type |
| zb_uint8_t | start_index |
Parameters for ieee_addr_req command.
| zb_uint16_t zb_zdo_ieee_addr_req_param_s::dst_addr |
Destination address
| zb_uint16_t zb_zdo_ieee_addr_req_param_s::nwk_addr |
NWK address that is used for IEEE address mapping.
| zb_uint8_t zb_zdo_ieee_addr_req_param_s::request_type |
Request type for this command: 0x00 Single device response 0x01 Extended response
| zb_uint8_t zb_zdo_ieee_addr_req_param_s::start_index |
If the Request type for this command is Extended response, the StartIndex provides the starting index for the requested elements of the associated devices list